大家好,
我使用的板子型号是MKL27Z64VLH4
现在我需要把flash划分为几个区域。
一个是boot区域,
一个是main区域,
内容是:从地址0开始boot,然后跳转到另外一个地址进入main
在我使用KinetisFlashTool 把我的boot下载到0地址以后,工具就自动断开然后reset,当我再次打开,连接上以后就下载不进去了,提示如下:
Connected to device successfully!
Collecting device information......
Device information is updated!
Start update progress......
Update directly without unlock device.
Updating image......
Error: Update image failed(Command disallowed when security is enabled.).
Update process is stopped by error.
请问怎么解决。
谢谢各位。
六一儿童节快乐。
BR
Bernerd
楼主你好!
KL27Z64VLH4 是带有片上ROM bootloader的,你没有用ROM bootloader而是直接用的flash bootloader吗?
那么你这个flash bootloader是怎么写的呢?是否是更新的时候先放到RAM里,然后直接更新应用程序呢?
其实使用KL27,建议你还是直接使用ROMbootloader, 具体的使用,你可以参考KBOOT2.0的Getting Started with the Kinetis ROM Bootloader.pdf文档:
NXP_Kinetis_Bootloader_2_0_0\doc
你先试下ROM bootloader,如果还有问题,欢迎继续交流!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------