By using latest KDS V3.2.0 to import existing projects (earlier KDS V1.1.1), it shows warnings as below:
Description | Resource | Path | Location | Type |
Invalid project path: Include path not found (C:\Freescale\KDS_v3\eclipse\ProcessorExpert\lib\Kinetis\pdd2\MK64FN1M0LL12\peripherals). | MicroDriverDBC002 | pathentry | Path Entry Problem |
Description | Resource | Path | Location | Type |
Invalid project path: Include path not found (C:\Freescale\KDS_v3\eclipse\ProcessorExpert\lib\Kinetis\pdd2\MK64FN1M0LL12\system). | MicroDriverDBC002 | pathentry | Path Entry Problem |
Is there any add-on for it?
And when building this project, it indicates one errors as below:
Description | Resource | Path | Location | Type |
cannot find -lMicroDriverDBC002 | ThreeButtonDemo | C/C++ Problem |
"MicroDriverDBC002" is one of the importing projects.
解決済! 解決策の投稿を見る。
Hello Felix
The paths are different in KDS 3.2. These two paths are changed into:
C:\Freescale\KDS_v3\eclipse\ProcessorExpert\Repositories\Kinetis_Repository\lib\Kinetis\pdd2\MK64FN1M0LL12\peripherals
C:\Freescale\KDS_v3\eclipse\ProcessorExpert\Repositories\Kinetis_Repository\lib\Kinetis\pdd2\MK64FN1M0LL12\system
Could you please check the compiler settings for include path as Erich relied?
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks!
It fixes the issues about include path.
And now I am looking on -l command line issue.
Hello Felix
The paths are different in KDS 3.2. These two paths are changed into:
C:\Freescale\KDS_v3\eclipse\ProcessorExpert\Repositories\Kinetis_Repository\lib\Kinetis\pdd2\MK64FN1M0LL12\peripherals
C:\Freescale\KDS_v3\eclipse\ProcessorExpert\Repositories\Kinetis_Repository\lib\Kinetis\pdd2\MK64FN1M0LL12\system
Could you please check the compiler settings for include path as Erich relied?
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Felix,
If I remember correctly, some directory/folder name have been chagned. You can remove these include paths from the projects settings.
Right click on the project > Properties > C/C++ Buld > Settings > Tool settings > Cross ARM C Compiler > Includes.
The second thinig with the build failing looks like somehow your command line (-I option) is wrong?
Erich