Try KDS 3.0.0 while keeping KDS 2.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Try KDS 3.0.0 while keeping KDS 2.0.0

408 次查看
jianluomath
Contributor I

I had converted an CW 10.06 project to KDS 2.0.0. The auto conversion didn't work well. I have to handcraft many things to get the project work with KDS 2.0.0.

Now, KDS 3.0.0 is out and I would like to try it out wile keeping the KDS 2.0.0 which I am currently using. Can I install KDS 3.0.0 without affecting my usage of

KDS 2.0.0?

标签 (1)
0 项奖励
回复
1 回复

273 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jian Luo:

Yes you can have both versions installed, I have not seen any problems, just DO NOT share the same workspace.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复