I had converted an CW 10.06 project to KDS 2.0.0. The auto conversion didn't work well. I have to handcraft many things to get the project work with KDS 2.0.0.
Now, KDS 3.0.0 is out and I would like to try it out wile keeping the KDS 2.0.0 which I am currently using. Can I install KDS 3.0.0 without affecting my usage of
KDS 2.0.0?
Hello Jian Luo:
Yes you can have both versions installed, I have not seen any problems, just DO NOT share the same workspace.
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------