KDS 3.0, MQX 4.2, GDB PE Micro Interface Debugging
Could not run gdb, does kds 3.0 support K60? Below are the error messages:
GNU gdb (GNU Tools for ARM Embedded Processors) 7.6.0.20140731-cvs
Copyright (C) 2013 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law. Type "show copying"
and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
monitor preserve0 0
monitor selectcore 0
Warning: the current language does not match this frame.
continue
Continuing.
Note: automatically using hardware breakpoints for read-only addresses.
Program received signal SIGTRAP, Trace/breakpoint trap.
0xfffffffe in ?? ()
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Connection from "127.0.0.1" via 127.0.0.1
Copyright 2012 P&E Microcomputer Systems,Inc.
Command Line :C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.2.5.201511061812\win32\pegdbserver_console -device=Freescale_K6x_K60FN1M0M12 -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=5000 -port=USB1
CMD>RE
Initializing.
Target has been RESET and is active.
CMD>CM C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.2.5.201511061812\win32\gdi\P&E\supportFiles_ARM\Freescale\K6x\freescale_k60fn1m0m12_1x32x256k_pflash.arp
Initializing.
Initialized.
;version 1.08, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [mk_1024k_n_pflash0_pflash1]
;device freescale, k60fn1m0m12, 1x32x256k, desc=pflash
;begin_cs device=$00000000, length=$00100000, ram=$20000000
Loading programming algorithm ...
Done.
CMD>EM
Erasing.
Module has been erased.
Initializing.
Initialized.
;version 1.08, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [mk_1024k_n_pflash0_pflash1]
;device freescale, k60fn1m0m12, 1x32x256k, desc=pflash
;begin_cs device=$00000000, length=$00100000, ram=$20000000
Loading programming algorithm ...
Done.
CMD>PM
Programming.
Processing Object File Data ...
.
Programmed.
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 00000400-0000040F ...
Ok.
block 00000420-00002117 ...
Ok.
Checksum Verification Successful. (Cumulative CRC-16=$154E)
CMD>RE
Initializing.
Target has been RESET and is active.
Fixed it. In the debug configuration, under Debugger tab, Advanced Options check the Non-Volatile Memory Preservation option to prevent overwriting the bootloader. In my case I preserved From: 0 To: ffff
Not sure how the Debug script got corrupted, but it did.
Did not work for me. See the message below:
GNU gdb (GNU Tools for ARM Embedded Processors) 7.6.0.20140731-cvs
Copyright (C) 2013 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law. Type "show copying"
and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
monitor preserve0 1 0 65535
monitor selectcore 0
Warning: the current language does not match this frame.
No source file named C:
Freescale
Freescale_MQX_4_2
mqx
examples
hello
hello.c.
continue
Continuing.
Note: automatically using hardware breakpoints for read-only addresses.
Program received signal SIGTRAP, Trace/breakpoint trap.
0xfffffffe in ?? ()
I don't have the Seeger Flasher. But I have no problem with the board using Code Warrior. I saw quite a few folks can use KDS 3.0 with this board. I probably missed something in my KDS or MQX 4.2 set up.
Have you tried the particular board using Code Warrior after getting the error with KDS 3.0? If it still works, then the bootloader is OK. So many things can mess up the bootloader, I’ve just got in the habit of re-flashing it whenever I see an error like the one you have.