Suspended : Signal : SIGTRAP:Trace/breakpoint trap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suspended : Signal : SIGTRAP:Trace/breakpoint trap

2,980件の閲覧回数
kayathrim
Contributor I

Hi all,

 

I have installed KDS 3.00 IDE. I am importing the KDS3 FSFK project from FreescaleSensorFusionRevision5. After Updating KDS, I am getting error like Suspended signal : SIGTRAP  during debugging. For selecting the device MK22FN1M0Axxx12  need to update the KDS. Is anyone faced the problem.

 

Regards,

Kayathri

ラベル(1)
0 件の賞賛
2 返答(返信)

2,047件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Kayathri,

At first , i recommend you create one simple project to have a try , if it is the same problem ,

please check the PE driver version on your PC , install the latest one .

If it still can not work ,please uninstalled the PEMicro Eclipse Plug-in from KDS, and re-installed it again .

PE Micro debugging issues with KDS and MKL03 microcontroller

If only the FSFK project can not work ,

What about the system frequency of your project ?

If too low , the P&E can't working well with low frequency, you can use J-link to instead to have a try .

Hope it helps

Alice

0 件の賞賛

2,047件の閲覧回数
kayathrim
Contributor I

Hi Alice,

Thank you for your suggestions. I have updated the KDS once again. FSFK project is working now.

Regards,

Kayathri

0 件の賞賛