Processor Expert - Build tries to create files in C:/Freescale/KDS_1.1.1 folder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert - Build tries to create files in C:/Freescale/KDS_1.1.1 folder

ソリューションへジャンプ
792件の閲覧回数
johnbaker
Contributor IV

I was trying to create a project using Processor Expert.  I created a new KDS workspace.  When creating the project I selected the 'Stand alone' option.  Why, when I try to build the project is it trying save PE generated code files in the KDS home folder instead of in my project folder in my workspace? (See attached snapshot).

 

Thanks,

 

John Baker

ラベル(1)
0 件の賞賛
返信
1 解決策
642件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It asks you to create (or copy from) the files on the left to the location on the right.

So the source of the file is in c:\freescale\kds_1.1.1/eclipse...... to your project subfolder Generated_Code/....

It should create the files inside your project structure, not in KDS.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
643件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It asks you to create (or copy from) the files on the left to the location on the right.

So the source of the file is in c:\freescale\kds_1.1.1/eclipse...... to your project subfolder Generated_Code/....

It should create the files inside your project structure, not in KDS.

Erich

0 件の賞賛
返信
642件の閲覧回数
johnbaker
Contributor IV

Thank Erich,    I guess I was just overly cautious.

John

0 件の賞賛
返信
642件の閲覧回数
johnbaker
Contributor IV

When I look at the Properties -> Processor Expert -> Generated code directory:  it points to 'Generated_Code' as it should.  (see attached snapshot)

Thanks,

John

0 件の賞賛
返信