Processor Expert - Build tries to create files in C:/Freescale/KDS_1.1.1 folder

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert - Build tries to create files in C:/Freescale/KDS_1.1.1 folder

跳至解决方案
739 次查看
johnbaker
Contributor IV

I was trying to create a project using Processor Expert.  I created a new KDS workspace.  When creating the project I selected the 'Stand alone' option.  Why, when I try to build the project is it trying save PE generated code files in the KDS home folder instead of in my project folder in my workspace? (See attached snapshot).

 

Thanks,

 

John Baker

标签 (1)
0 项奖励
回复
1 解答
589 次查看
BlackNight
NXP Employee
NXP Employee

It asks you to create (or copy from) the files on the left to the location on the right.

So the source of the file is in c:\freescale\kds_1.1.1/eclipse...... to your project subfolder Generated_Code/....

It should create the files inside your project structure, not in KDS.

Erich

在原帖中查看解决方案

0 项奖励
回复
3 回复数
590 次查看
BlackNight
NXP Employee
NXP Employee

It asks you to create (or copy from) the files on the left to the location on the right.

So the source of the file is in c:\freescale\kds_1.1.1/eclipse...... to your project subfolder Generated_Code/....

It should create the files inside your project structure, not in KDS.

Erich

0 项奖励
回复
589 次查看
johnbaker
Contributor IV

Thank Erich,    I guess I was just overly cautious.

John

0 项奖励
回复
589 次查看
johnbaker
Contributor IV

When I look at the Properties -> Processor Expert -> Generated code directory:  it points to 'Generated_Code' as it should.  (see attached snapshot)

Thanks,

John

0 项奖励
回复