I am new to KDS and Currently working MKE04Z8xxx4 controller. I need sample codes on serial communication(UART e.g., getchar(),putchar()),Timer delay functions(Similar to wait) I/O configurations and various other components. I was IAR and need some reference codes to develop sensor application and bootloader . Kindly provide any link or path ??
Hello ,
1. There are Typical Usage under the PE components :
also there are the UART APIs:
2. About the bootloader, there are two application note about UART bootloader and IIC bootloader
for kinetis E series, also have the source code :
http://cache.nxp.com/assets/documents/data/en/application-notes/AN4775.pdf?fsrch=1&sr=6&pageNum=1
http://cache.nxp.com/assets/documents/data/en/application-notes/AN4767.pdf?fsrch=1&sr=5&pageNum=1
Search AN4767sw and AN4775sw on NXP website can download the bootloader project .
3.About the sensor demo , there is a example for KE02, you can refer to it :
Processor Expert Guide for ADC to measure thermistor on KE02 Freedom board
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------