Hi,
I try to compile a KDS2 project with KDS3. The project is with K64F, KDSK110, Processeur Expert and MQX RTCS, under Windows7, I followed this post Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V... very usefull.
but I got some problem to solve the error below, it seems to be a problem with Semihosting, not sure,
make -j4 all
Building target: project_maf.elf
Invoking: Cross ARM C++ Linker
arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -T "L:/KDS3.0.0/ws_IDD4CLETHBt/project_maf/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"L:/KDS3.0.0/ws_IDD4CLETHBt/project_maf/Project_Settings/Linker_Files" -Wl,-Map,"project_maf.map" -nostartfiles -nodefaultlibs -nostdlib -Xlinker -z -Xlinker muldefs -Xlinker -static -specs=rdimon.specs -o "project_maf.elf" ./flash/CopyToRam.o ./flash/DEFlashPartition.o [...]
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-signalr.o): In function `_kill_r':
signalr.c:(.text._kill_r+0xe): undefined reference to `_kill'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-signalr.o): In function `_getpid_r':
signalr.c:(.text._getpid_r+0x0): undefined reference to `_getpid'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-writer.o): In function `_write_r':
writer.c:(.text._write_r+0x10): undefined reference to `_write'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-closer.o): In function `_close_r':
closer.c:(.text._close_r+0xc): undefined reference to `_close'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-fstatr.o): In function `_fstat_r':
fstatr.c:(.text._fstat_r+0xe): undefined reference to `_fstat'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-isattyr.o): In function `_isatty_r':
isattyr.c:(.text._isatty_r+0xc): undefined reference to `_isatty'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-lseekr.o): In function `_lseek_r':
lseekr.c:(.text._lseek_r+0x10): undefined reference to `_lseek'
C:/Freescale/KDS_3.0.0/eclipse//../toolchain/arm-none-eabi/lib/armv7e-m/fpu/libc.a(lib_a-readr.o): In function `_read_r':
readr.c:(.text._read_r+0x10): undefined reference to `_read'
collect2.exe: error: ld returned 1 exit status
makefile:98: recipe for target 'project_maf.elf' failed
make: *** [project_maf.elf] Error 1
I tried to add -specs=rdimon.specs and -specs=nosys.specs, I got same error messages.
Do you have any idea?
Regards
解決済! 解決策の投稿を見る。
Hi Bernard,
I think this in the linker options is your problem:
-nostartfiles -nodefaultlibs -nostdlib -Xlinker -z -Xlinker muldefs -Xlinker -static
With this, you say that the linker should not use the default libraries and standard libraries: I suggest you try this:
Not sure why you have the additional -Xinker options, are they needed by MQX?
Erich
Hi Bernard,
I think this in the linker options is your problem:
-nostartfiles -nodefaultlibs -nostdlib -Xlinker -z -Xlinker muldefs -Xlinker -static
With this, you say that the linker should not use the default libraries and standard libraries: I suggest you try this:
Not sure why you have the additional -Xinker options, are they needed by MQX?
Erich
hello,I have the same question,
but when I removed -nostartfiles -nodefaultlibs -nostdlib follow you
it don't outout the *.elf file only an a.out
and I can't download it to my board
could you help me??
'Building target: mytask_k64.elf'
'Invoking: Cross ARM C++ Linker'
arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -T E:\Freescale\KSDK_1.2.0\platform\devices\MK64F12\linker\gcc\MK64FN1M0xxx12_flash.ld -Xlinker --gc-sections -L"E:\Freescale\KSDK_1.2.0\lib\ksdk_mqx_lib\kds\K64F12\debug" -L"E:\Freescale\KSDK_1.2.0\lib\ksdk_platform_lib\kds\K64F12\debug -L"E:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\nshell" -L"E:\Freescale\KSDK_1.2.0\middleware\filesystem\mfs\lib\frdmk64f.kds\debug\mfs" -L"E:\Freescale\KSDK_1.2.0\middleware\tcpip\rtcs\lib\frdmk64f.kds\debug\rtcs" -L"E:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\mqx_stdlib" -L"E:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\mqx" -Wl,-Map,"mytask_k64.map" -Xlinker --cref --specs=nano.specs -Xlinker -static -Xlinker -z -Xlinker muldefs -Xlinker --undefined=__isr_vector -Xlinker --defsym=__stack_size__=0x400 -Xlinker --defsym=__heap_size__=0x200 -o "mytask_k64.elf" ./Sources/main.o ./KSDK_Files/board.o ./KSDK_Files/gpio_pins.o ./KSDK_Files/pin_mux.o ./Debug_Console/fsl_debug_console.o ./Debug_Console/fsl_misc_utilities.o ./Debug_Console/print_scan.o ./BSP_Files/init_bsp.o ./BSP_Files/mqx_main.o ./main.o E:/Freescale/KSDK_1.2.0/lib/ksdk_mqx_lib/kds/K64F12/debug/libksdk_platform_mqx.a E:/Freescale/KSDK_1.2.0/middleware/tcpip/rtcs/lib/frdmk64f.kds/debug/rtcs/lib_rtcs.a E:/Freescale/KSDK_1.2.0/lib/ksdk_platform_lib/kds/K64F12/debug/libksdk_platform.a E:/Freescale/KSDK_1.2.0/middleware/filesystem/mfs/lib/frdmk64f.kds/debug/mfs/lib_mfs.a E:/Freescale/KSDK_1.2.0/rtos/mqx/lib/frdmk64f.kds/debug/nshell/lib_nshell.a E:/Freescale/KSDK_1.2.0/rtos/mqx/lib/frdmk64f.kds/debug/mqx_stdlib/lib_mqx_stdlib.a E:/Freescale/KSDK_1.2.0/rtos/mqx/lib/frdmk64f.kds/debug/mqx/lib_mqx.a -lksdk_platform_mqx -l_mqx_stdlib -l_mqx -lgcc -lc -lsupc++ -lm -lnosys
e:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/bin/ld.exe: warning: cannot find entry symbol Reset_Handler; defaulting to 00000410
'Finished building target: mytask_k64.elf'
Erich Styger kirjoitti:
I think this in the linker options is your problem:
-nostartfiles -nodefaultlibs -nostdlib -Xlinker -z -Xlinker muldefs -Xlinker -static
Not sure why you have the additional -Xinker options, are they needed by MQX?
I also experienced this after installing KDS3.0 alongside KDS2.0
After trying KDS3.0, all my projects in KDS2.0 workspace got those odd options, and failed to compile.
Also, the checkboxes you highlighted were not checked, but the -nostartfiles etc options were added directly to the text field on the Miscellaneous tab.
Hi Erich,
Yes, you are good.
I removed -nostartfiles -nodefaultlibs -nostdlib
and add -specs=rdimon.specs
I got no errors, cool.
Bernard