MKW01Z128 support in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKW01Z128 support in KDS

638件の閲覧回数
paulkurucz
Contributor I

I was wondering if anyone out there was targeting the MKW01Z128 with KDS.    And if so is the MKL15Z128xxx4 the closest core variant in KDS that lines up with the MKW01Z128?

 

Thanks,

 

Paul

ラベル(1)
タグ(2)
0 件の賞賛
4 返答(返信)

441件の閲覧回数
jasveersingh
Contributor I

Even I am targeting the MKW01Z128 with KDS. Have just bought the freedom board FRDM-KW019032 but do not know how KDS can be used for the same.

0 件の賞賛

441件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jasveer,

Yes, the KDS support this chip .

pastedImage_0.png

Hope it helps
Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

441件の閲覧回数
jasveersingh
Contributor I

Thank you Alice, that is helpful. But as I checked KDS doesnt support the FRDM-KW019032 under the boards category, so does that mean I will not be able to program the board? What is the difference in having a board project & a processor project in KDS?

0 件の賞賛

441件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jasveer,

We can use the KDS develop the board of FRDM-KW019032 .

On KDS , select the"board " and "processor" boards are OK , it doesn't matter .

In generally , i select the "processor" .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛