Launching screen hangs on 94%

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Launching screen hangs on 94%

ソリューションへジャンプ
1,869件の閲覧回数
neilporven
Senior Contributor I

I am getting hanged up on the following screen:

 

145968_145968.jpgLaunching.jpg

 

It stays at 94% and never continues past this.  I also find it annoying that the Cancel button doesn't respond

once pressed. 

By the way, the software compiles without errors and I tried re-building it several times and have also done

a clean on it.  If I load another software, it seems to load fine, so there isn't a hardware/multilink issue with

the board.

Can someone explain why this is happening?

 

Thanks,

Neil Porven

ラベル(1)
0 件の賞賛
返信
1 解決策
3 返答(返信)
1,719件の閲覧回数
neilporven
Senior Contributor I

Hi Erich,

I followed the link you sent me and it described the issue, exactly!  I followed your fix and sure enough, the debug execution

completed all the way through.  

Excellent, thank you much.

I will update my KDS to 3.2.0 to avoid this in the future.

Neil

0 件の賞賛
返信
1,719件の閲覧回数
neilporven
Senior Contributor I

Thank you Erich,

Quick update, if you want to see the code and experience the issue.

I am using the following:

C:\Freescale\SDK_2.0_K64F\boards\frdmk64f\driver_examples\sdcard\polling\kds

Just load that, compile it, plug in your P&E to your FRDMK64F evaluation board and you should

see what I am seeing.

Neil

0 件の賞賛
返信