Kinetis Design Studio creates "Processor Expert" and "MyComponents" folders in my home folder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio creates "Processor Expert" and "MyComponents" folders in my home folder

1,187件の閲覧回数
arjunnair
Contributor II

Dear all,

I run OpenSuse Tumbleweed on my computer.

I do not want to clutter my home folder with "Processor Expert" and "MyComponents" folders. These folders are recreated every time I start KDS. I tried to look for some path variable that I could change to move these folders to another location and failed. Does anybody have a solution for this?

Thank you.

ラベル(1)
0 件の賞賛
5 返答(返信)

969件の閲覧回数
liborukropec
NXP Employee
NXP Employee

What you can try is to set the environment variable "ALLUSERSPROFILE" to existing folder where the user has write access, e.g. something like this:

mkdir /opt/expertwritablearea
export ALLUSERSPROFILE=/opt/expertwritablearea
./kinetis-design-studio‍‍‍

I did not test but I expect it will work.

Regards,

Libor

0 件の賞賛

969件の閲覧回数
arjunnair
Contributor II

I tried to export 'ALLUSERPROFILE' and 'home_ProcessorExpert_loc' to another folder. It doesn't work.

0 件の賞賛

969件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello,

you have a typo - missing "S" after word USER. Correct version is below:

export ALLUSERPROFILE=/tmp/pex
./kinetis-design-studio

I just verified it works with KDS 3.2.0. The directory in the env. variable is automatically created (if pointed to the place where the user has the appropriate rights.

It is also visible in the Processor Expert console:

pastedImage_1.png

Hope it helps,

Libor

0 件の賞賛

969件の閲覧回数
BlackNight
NXP Employee
NXP Employee

There is a setting here:

pastedImage_1.png

At least for the 'MyComponents'.

I hope this helps,

Erich

0 件の賞賛

969件の閲覧回数
arjunnair
Contributor II

Hi Erich,

Thanks. Unfortunately, that doesn't help. It isn't possible to edit the path.

pastedImage_1.png

0 件の賞賛