KDS on OS X El Capitan (Beta)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS on OS X El Capitan (Beta)

3,993件の閲覧回数
valentinpy
Contributor I

Hello,

 

If someone is trying to use/install KDS v3.0 on the public beta (4) of OS X El Capitan (10.11), you'll probably have a problem at the workspace selection.

As i found no information about this on the Internet, but solved the problem, here is my solution.

 

To resolve this problem, I modified the file located here:

"/Applications/KDS_3.0.0.app/Contents/eclipse/kinetis-design-studio.ini" and removed the lines 7 and 8:

 

To delete:

-showSplash

com.somniumtech.branding.kds

 

Modified file:

-startup

plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar

--launcher.library

plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.1.200.v20150204-1316

-product

com.somniumtech.branding.kds.ide

--launcher.defaultAction

openFile

-name

Kinetis Design Studio

--launcher.XXMaxPermSize

256m

-vm

features/com.somniumtech.jre.macosx.cocoa.x86_64_1.7.0.76/jre/Contents/Home/lib/jli/libjli.dylib

-vmargs

-Dosgi.requiredJavaVersion=1.7

-Xms256m

-Xmx512m

-XX:PermSize=256m

-XX:MaxPermSize=512m

-XstartOnFirstThread

-Dorg.eclipse.swt.internal.carbon.smallFonts

 

With that modification, the splash screen is not display and you should be able to choose you workspace and use KDS.

ラベル(1)
タグ(3)
13 返答(返信)

1,863件の閲覧回数
mstroven
Contributor III

Thank you so much!

0 件の賞賛

1,863件の閲覧回数
victorperez
Contributor I

Huge Help.  Thank you!

0 件の賞賛

1,863件の閲覧回数
markbereit
Contributor I

Hooray!  Your post rescued me, too!

(Hoping the next update to KDS addresses whatever problem this is, but in the mean time, thank you!)

0 件の賞賛

1,863件の閲覧回数
nestordamiangar
Contributor II

Thanks it worked for me as well

0 件の賞賛

1,863件の閲覧回数
JonathanHess
Contributor III

Yay!

0 件の賞賛

1,863件の閲覧回数
solen
Contributor II

Thanks! Worked for me as well!

0 件の賞賛

1,863件の閲覧回数
allenantony
Contributor II

Worked like a charm!

0 件の賞賛

1,863件の閲覧回数
jrychter
Contributor V

Thanks for posting this!

0 件の賞賛

1,863件の閲覧回数
berrymoist
Contributor I

Thank you very much.

0 件の賞賛

1,863件の閲覧回数
kladu
Contributor II

Works. Thank you!

0 件の賞賛

1,863件の閲覧回数
nirvanauscn
Contributor III

The suggestion works for me with the formal El Capitan released last week.

1,863件の閲覧回数
vcanuel
Contributor II

Thanks :smileyhappy:

0 件の賞賛

1,863件の閲覧回数
aussiemate
Contributor II

Thank you so much for that comment. 

Was sitting here with a "DeaD" KDS on El Capitan beta 8, which locked up after the splash screen had disappeared, did what you suggested and now works.