Hello,
If someone is trying to use/install KDS v3.0 on the public beta (4) of OS X El Capitan (10.11), you'll probably have a problem at the workspace selection.
As i found no information about this on the Internet, but solved the problem, here is my solution.
To resolve this problem, I modified the file located here:
"/Applications/KDS_3.0.0.app/Contents/eclipse/kinetis-design-studio.ini" and removed the lines 7 and 8:
To delete:
-showSplash
com.somniumtech.branding.kds
Modified file:
-startup
plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar
--launcher.library
plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.1.200.v20150204-1316
-product
com.somniumtech.branding.kds.ide
--launcher.defaultAction
openFile
-name
Kinetis Design Studio
--launcher.XXMaxPermSize
256m
-vm
features/com.somniumtech.jre.macosx.cocoa.x86_64_1.7.0.76/jre/Contents/Home/lib/jli/libjli.dylib
-vmargs
-Dosgi.requiredJavaVersion=1.7
-Xms256m
-Xmx512m
-XX:PermSize=256m
-XX:MaxPermSize=512m
-XstartOnFirstThread
-Dorg.eclipse.swt.internal.carbon.smallFonts
With that modification, the splash screen is not display and you should be able to choose you workspace and use KDS.
Hooray! Your post rescued me, too!
(Hoping the next update to KDS addresses whatever problem this is, but in the mean time, thank you!)