Good morning
I have a project, and the linking process is looking for a wrong file.
The project has the SDK 1.3 included as source code, not a library. the compilation goes straight but the linker is looking for the fl_gpio_driver.o in place of the fsl_gpio_driver.o . I don t understand where this name is coming from.
In the attached video a view of the what it is happening...
Needed help
Thank You
解決済! 解決策の投稿を見る。
Yes, there is a limit of 8192 characters on Windows (see https://mcuoneclipse.com/2015/03/29/solving-the-8192-character-command-line-limit-on-windows/ ). KDS V3.2.0 has that solution included, so you can use longer than 8192 command lines to the GNU tools. As an FYI, there is still an issue if you do a 'clean' command, but you can manually delete the output files if needed.
I hope this helps,
Erich
I am trying to play removing from the building some files. The problem changes but still problem.
Now I dump the command line of the linker in the attached file, with the error message.
There is no sense. it seems it is looking for a file path not in the command line. "platfrm" in place of "platform"
Is there a limit in the length of the command line ???
Maybe too long ??
Yes, there is a limit of 8192 characters on Windows (see https://mcuoneclipse.com/2015/03/29/solving-the-8192-character-command-line-limit-on-windows/ ). KDS V3.2.0 has that solution included, so you can use longer than 8192 command lines to the GNU tools. As an FYI, there is still an issue if you do a 'clean' command, but you can manually delete the output files if needed.
I hope this helps,
Erich
I installed the 3.2.0
The linking is proceeding...
Thank You
Thank You, Always quick to help..
I have now the KDS 3.0.0.
I need to update to go further...???