I am installing KDS on Ubuntu. The intent is to develop software for FRDM-KW41Z. I have followed the LInux installation instructions in the Kinetis Design Studio 3.2.0 Release Notes.
xxx@bill-ThinkPad-T440:~$ lsb_release -a
No LSB modules are available.
Distributor ID: Ubuntu
Description: Ubuntu 14.04.5 LTS
Release: 14.04
Codename: trusty
...
xxx@bill-ThinkPad-T440:~/Projects$ ls kin*
kinetis-design-studio_3.2.0-1_amd64.deb
xxx@bill-ThinkPad-T440:~/Projects$ sudo dpkg -i kinetis-design-studio_3.2.0-1_amd64.deb
(Reading database ... 853393 files and directories currently installed.)
Preparing to unpack kinetis-design-studio_3.2.0-1_amd64.deb ...
Unpacking kinetis-design-studio (3.2.0) over (3.2.0) ...
Setting up kinetis-design-studio (3.2.0) ...
**********************************************************************
* Warning: This package includes the GCC ARM Embedded toolchain, *
* which is built for 32-bit hosts. If you are using a *
* 64-bit system, you may need to install additional *
* packages before building software with these tools. *
* *
* For more details see: *
* - KDS_Users_Guide.pdf:"Installing Kinetis Design Studio". *
* - The Kinetis Design Studio release notes. *
**********************************************************************
Processing triggers for gnome-menus (3.10.1-0ubuntu2) ...
Processing triggers for desktop-file-utils (0.22-1ubuntu1) ...
Processing triggers for bamfdaemon (0.5.1+14.04.20140409-0ubuntu1) ...
Rebuilding /usr/share/applications/bamf-2.index...
Processing triggers for mime-support (3.54ubuntu1.1) ...
xxx@bill-ThinkPad-T440:~/Projects$ cd /opt/Freescale
xxx@bill-ThinkPad-T440:/opt/Freescale$ ls -l
total 0
I am expecting to find the installed files in /opt/Freescale, but it's empty.
已解决! 转到解答。
Hello, Robert!
I ran into the same problem. How I fixed it:
sudo dpkg --remove kinetis-design-studio
to remove any failed installation. Then I ran the command again:
sudo dpkg -i kinetis-design-studio_3.2.0-1_amd64.deb
and it passed.
It actually succeeded the first time, but I wanted to reinstall it and ran into the problem you have.
Further more - after the successful install I updated the segger drivers cus it turns out they are a bit old (follow this link Updating Segger Tools in Eclipse Kinetis Design Studio | MCU on Eclipse )
hope this helps!
Hello, Robert!
I ran into the same problem. How I fixed it:
sudo dpkg --remove kinetis-design-studio
to remove any failed installation. Then I ran the command again:
sudo dpkg -i kinetis-design-studio_3.2.0-1_amd64.deb
and it passed.
It actually succeeded the first time, but I wanted to reinstall it and ran into the problem you have.
Further more - after the successful install I updated the segger drivers cus it turns out they are a bit old (follow this link Updating Segger Tools in Eclipse Kinetis Design Studio | MCU on Eclipse )
hope this helps!