Hi,
Today, I have done a restore defaults in C/C++ Build\Settings in my project for mistake.
After configure some old settings, the printing size and create flash Image didn't work even if selected.
I can't understand what is the problem..Can someone help me.
Best Regards,
Hi Erich,
Thank you for your help.
I detect a diference beteween the old makefile and the current.
It looks like the following line is missing: secondary-outputs: $(SECONDARY_FLASH) $(SECONDARY_SIZE).
But i can't set this option on make file.
Are you using custom build settings? If yes, then this could be the solution for you: Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse
Otherwise please share more information (e.g. the console output text you get).
I hope this helps,
Erich