KDS 3.2.0 printing size problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.2.0 printing size problem

669件の閲覧回数
brunoaguiam
Contributor I

Hi,

Today, I have done a restore defaults in C/C++ Build\Settings in my project for mistake.

After configure some old settings, the printing size and create flash Image didn't work even if selected.

I can't understand what is the problem..Can someone help me.

Best Regards,

0 件の賞賛
返信
3 返答(返信)

599件の閲覧回数
brunoaguiam
Contributor I

Hi Erich,

Thank you for your help.

I detect a diference beteween the old makefile and the current.

It looks like the following line is missing: secondary-outputs: $(SECONDARY_FLASH) $(SECONDARY_SIZE).

But i can't set this option on make file.

0 件の賞賛
返信

599件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Bruno,

are you able to share your project?

Erich

0 件の賞賛
返信

599件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Are you using custom build settings? If yes, then this could be the solution for you: Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse 

Otherwise please share more information (e.g. the console output text you get).

I hope this helps,

Erich

0 件の賞賛
返信