KDS 3.0 compiler error "fsl_gpio_driver.h"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.0 compiler error "fsl_gpio_driver.h"

464件の閲覧回数
joaquimmartine1
Contributor I

Hi everyone,

 

I just installed the KDS 3.0.0 in order to run the "quick start demo " of FRDM-K22F.

 

When I compile there is an error: the file "fsl_gpio_driver.h" is not found.

 

I read the post KDS problem with K22f about this. I have configured the path but I think the file is missed, because I can't found the file neither the project not KDS paths.

 

Please, can anybody help me on this.

 

Thank you in advance.

 

56819_56819.pngpastedImage_0.png

 

56820_56820.pngpastedImage_2.png

ラベル(1)
0 件の賞賛
1 返信

299件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Joaquim,

Please be sure that under the option Properties > C/C++ Build > Settings > Cross ARM C Compiler > Includes > Include paths (-I) is included the path C:\Freescale\KSDK_1.2.0\platform\drivers\inc.

Best regards,

Earl Orlando.

0 件の賞賛