Gnu loader cant find built MQX 4.1 files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Gnu loader cant find built MQX 4.1 files

跳至解决方案
1,455 次查看
kcw
Contributor III

Is anyone else having this issue?

 


'Building target: test_kds_2.elf'

'Invoking: Cross ARM C++ Linker'

arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -T "C:/workspace_kds/test_kds_2/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"C:/workspace_kds/test_kds_2/Project_Settings/Linker_Files" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\usb" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\shell" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\rtcs" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\psp" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\mfs" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp\Sources" -L"C:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp\Generated_Code" -Wl,-Map,"test_kds_2.map" -v -nanolibc -o "test_kds_2.elf"  ./Sources/Events.o ./Sources/Tasks.o ./Sources/main.o ./Sources/my_tasks.o  ./Project_Settings/Startup_Code/startup.o  ./Generated_Code/System/CPU_Init.o ./Generated_Code/System/Peripherals_Init.o ./Generated_Code/System/Vectors.o  ./Generated_Code/Cpu.o ./Generated_Code/GPIO1.o ./Generated_Code/GPIO2.o ./Generated_Code/MQX1.o ./Generated_Code/PE_LDD.o ./Generated_Code/pin_mux.o   -l"usb.a" -l"shell.a" -l"rtcs.a" -l"psp.a" -l"mfs.a" -l"bsp.a"

 

 

Using built-in specs.

COLLECT_GCC=arm-none-eabi-g++

COLLECT_LTO_WRAPPER=c:/freescale/kds_1.1.0/toolchain/bin/../libexec/gcc/arm-none-eabi/4.8.0/lto-wrapper.exe

Target: arm-none-eabi

 

Configured with: /work/joes/kds-releases/1.1.0/src/gcc-4.8-kiln/configure --build=i686-unknown-linux-gnu --disable-libssp --disable-nls --disable-plugin --enable-languages=c,c++ --host=i686-w64-mingw32 --htmldir=/opt/Freescale/KDS_1.1.0/doc/html/gcc --infodir=/opt/Freescale/KDS_1.1.0/doc/info/gcc --mandir=/opt/Freescale/KDS_1.1.0/doc/man/gcc --pdfdir=/opt/Freescale/KDS_1.1.0/doc/pdf/gcc --prefix=/opt/Freescale/KDS_1.1.0/toolchain --target=arm-none-eabi --with-bugurl='Freescale Support <support@freescale.com>' --with-cpu=cortex-m0 --with-gmp=/work/joes/kds-releases/1.1.0/obj/host_i686-w64-mingw32/gmp/somn_install --with-mode=thumb --with-mpc=/work/joes/kds-releases/1.1.0/obj/host_i686-w64-mingw32/mpc/somn_install --with-mpfr=/work/joes/kds-releases/1.1.0/obj/host_i686-w64-mingw32/mpfr/somn_install --with-newlib --with-pkgversion='Kinetis Design Studio v1.1.0' --with-sysroot=/work/joes/kds-releases/1.1.0/install/i686-w64-mingw32/arm-none-eabi

 

(i am not sure where this came from. no such directory on my system)

 

Thread model: single

 

gcc version 4.8.0 (Kinetis Design Studio v1.1.0)

COMPILER_PATH=c:/freescale/kds_1.1.0/toolchain/bin/../libexec/gcc/arm-none-eabi/4.8.0/;c:/freescale/kds_1.1.0/toolchain/bin/../libexec/gcc/;c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/

LIBRARY_PATH=c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/m4/fp/v4-sp-d16/;c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/lib/m4/fp/v4-sp-d16/;c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/;c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/;c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/lib/

COLLECT_GCC_OPTIONS='-mcpu=cortex-m4' '-mthumb' '-mfloat-abi=hard' '-mfpu=fpv4-sp-d16' '-O0' '-fmessage-length=0' '-fsigned-char' '-ffunction-sections' '-fdata-sections' '-g3' '-T' 'C:/workspace_kds/test_kds_2/Project_Settings/Linker_Files/ProcessorExpert.ld' '-LC:/workspace_kds/test_kds_2/Project_Settings/Linker_Files' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\usb' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\shell' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\rtcs' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\psp' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\mfs' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp\Sources' '-LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp\Generated_Code' '-v' '-nanolibc' '-o' 'test_kds_2.elf'

 

c:/freescale/kds_1.1.0/toolchain/bin/../libexec/gcc/arm-none-eabi/4.8.0/collect2.exe --sysroot=/work/joes/kds-releases/1.1.0/install/i686-w64-mingw32/arm-none-eabi -X -o test_kds_2.elf c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/m4/fp/v4-sp-d16/crti.o c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/m4/fp/v4-sp-d16/crtbegin.o c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/lib/m4/fp/v4-sp-d16/crt0.o -LC:/workspace_kds/test_kds_2/Project_Settings/Linker_Files -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\usb -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\shell -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\rtcs -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\psp -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\mfs -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp\Sources -LC:\Freescale\Freescale_MQX_4_1\lib\frdmk64f.kds\debug\bsp\Generated_Code -Lc:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/m4/fp/v4-sp-d16 -Lc:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/lib/m4/fp/v4-sp-d16 -Lc:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0 -Lc:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc -Lc:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/lib --gc-sections -Map test_kds_2.map ./Sources/Events.o ./Sources/Tasks.o ./Sources/main.o ./Sources/my_tasks.o ./Project_Settings/Startup_Code/startup.o ./Generated_Code/System/CPU_Init.o ./Generated_Code/System/Peripherals_Init.o ./Generated_Code/System/Vectors.o ./Generated_Code/Cpu.o ./Generated_Code/GPIO1.o ./Generated_Code/GPIO2.o ./Generated_Code/MQX1.o ./Generated_Code/PE_LDD.o ./Generated_Code/pin_mux.o -lusb.a -lshell.a -lrtcs.a -lpsp.a -lmfs.a -lbsp.a -lstdc++ -lm --start-group -lgcc -lg_s -lc_s --end-group c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/m4/fp/v4-sp-d16/crtend.o c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/m4/fp/v4-sp-d16/crtn.o -T C:/workspace_kds/test_kds_2/Project_Settings/Linker_Files/ProcessorExpert.ld


c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lusb.a

c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lshell.a

c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lrtcs.a

c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lpsp.a

c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lmfs.a

c:/freescale/kds_1.1.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.0/../../../../arm-none-eabi/bin/ld.exe: cannot find -lbsp.a

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,148 次查看
kcw
Contributor III

The arm-none-eabi-g++ requires the libaryname file to be named "liblibaryname.a"

kds and arm-none-eabi-gcc generate a file with "libaryname.a"

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,148 次查看
lvw
Contributor II

You have to import all used libraries (psp, bsp, shell, etc...) in KDS and to build them. It will create all these missing files.

See in <MQX>\doc\tools\kds\MQX_KDS_Getting_Started.pdf.

1,149 次查看
kcw
Contributor III

The arm-none-eabi-g++ requires the libaryname file to be named "liblibaryname.a"

kds and arm-none-eabi-gcc generate a file with "libaryname.a"

0 项奖励
回复