Hi All
I have been using the GCC compiler version which was installed with KDS 1.0.1 for some time.
A few days ago I updated to KDS 1.1.1 and deinstalled KDS 1.0.1.
Today I had a shock. A project that was building to a size of 98k Flash using the GCC version from KDS 1.0.1 now builds to 120k Flash, using the same settings as before (-Os) [when build with the GCC version in KDS 1.1.1].
The deinstallation has deleted the old GCC binaries and KDS 1.0.1 is no longer available for download.
Are different settings required with the GCC version now used to make it efficient again?
Regards
Mark