Can we use the ULINK2 JTAG ICE debugger?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we use the ULINK2 JTAG ICE debugger?

3,620件の閲覧回数
isaotakashima
Contributor IV

We have the ULINK2 JTAG ICE debugger. And we want to use the Kinetis Design Studio (KDS) IDE.

We make the new project using KDS, it project include settings of the following JTAG ICE.

- GDB hardware Debugging

- GDB OpenOCD Debugging

- GDB PEMicro Interface Debugging

- GDB SEGGER J-Link Debugging

Unfortunately, it project does not include settings for the ULINK2.

Please let us know how to add  settings for the ULINK2.

 

Best regards,

Takashima

ラベル(1)
タグ(2)
1 返信

1,847件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Takashima,

you would need a GDB server for the ULINK2.

See ULINK2 USB-JTAG with Gnu ARM toolchain

So to my knowledge the ULINK2 can only be used with Keil, and not with GDB.

Erich

0 件の賞賛
返信