EZPORT with mbed and KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EZPORT with mbed and KDS

870件の閲覧回数
JonathanHess
Contributor III

I've successfully created a project that started from a KDS export of mbed blinky for a FRDM-K64F!

 

Now it is time to cut the USB umbilical but a cold power on doesn't reset properly.  I have switched the reset selection jumper.  Sounds a whole lot like:

 

FRDM-K64F booting issue when powered from USB port

 

But... my KDS project has no .s files but it does have a startup_MK64F12.o.  Any ideas on the easiest way to tweak the EZPORT bit?

ラベル(1)
0 件の賞賛
2 返答(返信)

496件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Jon,

The  startrup_MK64F12.s file is here :

3.png

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 件の賞賛

496件の閲覧回数
JonathanHess
Contributor III

I got my project as a KDS export from the mbed online compiler.  As such, It only had .o files.  I tried getting the source from:

     http://developer.mbed.org/users/mbed_official/code/mbed-src/export

I moved the existing mbed directory out of my project directory.  Moved the new source dump in.  Started up kds and told it to resync but now I'm having project issues.

Thanks,

Jonathan

0 件の賞賛