I used the following ld code successfully on an earlier K22 project to link in the binary of a bootloader.
/********************************************/
MEMORY
{
m_boot (RX) : ORIGIN = 0x00000000, LENGTH = 0x00008000
m_interrupts (RX) : ORIGIN = 0x00008000, LENGTH = 0x00000400
m_text (RX) : ORIGIN = 0x00008400, LENGTH = 0x00077C00
m_flash_nvm (RX) : ORIGIN = 0x10000000, LENGTH = 0x00020000
m_flex_ram (RX) : ORIGIN = 0x14000000, LENGTH = 0x00001000
m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x0000FC00
m_stack (RW) : ORIGIN = 0x1FFFFC00, LENGTH = 0x400
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000
m_bbram (RW) : ORIGIN = 0xA0000000, LENGTH = 0x00080000
}
HEAP_SIZE = 0xFC00;
STACK_SIZE = 0x0400;
M_VECTOR_RAM_SIZE = 0x0;
TARGET(binary)
INPUT(bootloader.bin)
OUTPUT_FORMAT(default)
/* Define output sections */
SECTIONS
{
.boot :
{
bootloader.bin (.data)
. = ALIGN(4);
} >m_boot
/* The startup code goes first into internal flash */
.interrupts :
etc.
/********************************************/
But now I am trying to link a .bmp file in a KL33 project with no luck using the following link script:
/********************************************/
TARGET(binary)
INPUT(Icon.bmp)
OUTPUT_FORMAT(default)
/* Define output sections */
SECTIONS
{
/* The startup code goes first into internal flash */
.interrupts :
{
__VECTOR_TABLE = .;
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} > m_interrupts
.flash_config :
{
. = ALIGN(4);
KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */
. = ALIGN(4);
} > m_flash_config
.bitmaps :
{
. = ALIGN(4);
Icon.bmp (.data)
} >m_text
/********************************************/
The first error of several I get is:
ZS.elf section `.data' will not fit in region `m_data'
I have commented out the .bitmaps section, and even commented out the INPUT(Icon.bmp) line and still get the error. So it must have something to do with the TARGET() and/or OUTPUT_FORMAT() commands? Any help would be appreciated.
Hello Michael,
- The error message "`.data' will not fit in region `m_data'" , it shows the .data overflow m_data section,
i think in your linker file , there is a section like :
.data:
{
...
}>m_data
So please send your linker file and .map file to me , or you can check the .map file by yourself to find
which data overflow , or too large .
- Please pay attention to that, the memory map is difference between K22 and KL33 .
-And i have a question , does these function out put to console or UART in your project ?
INPUT(Icon.bmp)
OUTPUT_FORMAT(default)
Hope it helps
Alice
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Alice,
Please see
to see where I originally learned how to merge a bootloader with my K22
application.
I thought it would carry over, but it didn't.
TARGET, INPUT, and OUTPUT_FORMAT are ld script commands controlling
files that can be input to the gcc linker. I got them from the "Merging
applications using Kinetis Design Studio.pdf" document.
Through trial and error, I was able to get the linker to work for the
KL33 project by changing the OUTPUT_FORMAT(default) command to
TARGET(default). I don't know why.
Mike
Hi Mike,
Thanks for your sharing, i have not test this tutorial.
For size of KL33 RAM is smaller than K22, so maybe the "OUTPUT_FORMAT(default)"
need more RAM usage, so it overflow . In the error message, does it show what the size overflowed?
BR
Alice
Alice,
The console log is attached for when I changed TARGET(default) back to
OUTPUT_FORMAT(default) in the .ld file.
There is no mention of "overflow" now, nor is there a .map file
generated. But I do remember getting a .map file before, maybe in some
other trial and error attempt. The .map file then showed m_data overflow.
I don't remember all the details anymore, only that it is now working
with TARGET(default).
Mike