lpc5506 keil通过jlink烧写之后黑屏

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc5506 keil通过jlink烧写之后黑屏

Jump to solution
1,952 Views
papa
Contributor I

我用gui guider 生成keil工程文件之后,通过j-link烧录,提示烧录成功后屏幕并没有显示,这是为什么呢?

0 Kudos
Reply
1 Solution
1,755 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

Sorry the GUI Guider doesn't support this board so far, recommend you development based on application you mentioned, it includes drivers for your board.

 

BR

Alice

 

View solution in original post

0 Kudos
Reply
8 Replies
1,912 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

 

你在SDK下找一个GUI guider 的 demo, 烧写进去,查看是否能正常显示。

 

BR

Alice

0 Kudos
Reply
1,897 Views
papa
Contributor I

我烧录官方发来的keil版本的示例程序是正常的,但是gui guider生成的示例程序不能显示,keil和MCUXpresso IDE都不行

0 Kudos
Reply
1,825 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

Could you please take a screenshot or video about the steps you create project and configuration.

 

BR

Alice

0 Kudos
Reply
1,808 Views
papa
Contributor I

I'm so sorry

For some reason, I couldn't upload the original

3f55dfe3434939902b437ac5df49ac3.jpg微信图片_20230522150651.jpg微信图片_20230522150805.jpg微信图片_20230522150905.jpgf44a6733cc04a15c51e3366da36c094.jpg微信图片_20230522151133.jpg微信图片_20230522151312.jpg微信图片_20230522151315.jpg

 

微信图片_20230522141706.jpg

0 Kudos
Reply
1,793 Views
LiubinGong
NXP Employee
NXP Employee

Hello  

  I'm guessing the root cause is a different panel

  1. We support LPC55s06, and the default panel adafruit-1947(320x240)
  2. Which board in the chosen SDK does it work?  would you please check the panel name and size?

Best Regards 

Liubin

0 Kudos
Reply
1,782 Views
papa
Contributor I

Hello LiubinGong

微信图片_20230522181250.jpg微信图片_20230522181305.jpgThis is what I ported the generated program to the demonstration program.

The initial panel size was adafruit-1947(320x240), but the scale was wrong.

So I'll change the panel size to 480 * 320,as shown in the figure.

0 Kudos
Reply
1,756 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

Sorry the GUI Guider doesn't support this board so far, recommend you development based on application you mentioned, it includes drivers for your board.

 

BR

Alice

 

0 Kudos
Reply
1,751 Views
papa
Contributor I
Oh, all right.
0 Kudos
Reply