want to use Freemaster to monitor and calibrate variables on the S32K144 via CAN, but I'm having trouble effectively configuring the CAN connection in Freemaster (see the illustration). Can you tell me how to solve this problem? Or is there a configuration manual or user guide available?
Hi @fengba_360 ,
It seems that the corresponding CAN probe driver is either not detected or is not compatible with FreeMASTER.
What CAN adapter are you using ?
Please note that CAN adapter software (driver) should be installed separately of FreeMASTER.
I reinstalled the ZLG CAN driver, and now FreeMASTER can recognize it, but it reports the error shown in the image. Can you tell me how to deal with it?
In most cases this error code means that FreeMASTER (desktop tool) did not receive a reply from the target board.
You would need to check whether CAN interface and FreeMASTER Driver are properly configured.
If you are using SDK to configure the CAN, you may need to disable transmission abort mechanism (see this thread for more info).
It's available on FreeMASTER's home page in downloads section. Here's a direct link.
If you are using S32 Design Studio, it is already included in S32K1xx development package - you can find it in `C:\NXP\S32DS.3.5\S32DS\software\FreeMASTER_Serial_Communication_Driver_V2_0`.
I would also recommend checking the following post - it explains UART configuration, but the same flow applies in case of CAN communication.