Freemaster response timeout with MPC5744P and AN12017

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Freemaster response timeout with MPC5744P and AN12017

跳至解决方案
1,164 次查看
eusebiu_bivol
Contributor II

Hello everyone,

I have just bought an MPC5744P devkit and I am trying to establish a Freemaster connection running the AN12017 (3-phase PMSM control) on it. I do not own the additional HW, therefore I have commented out the output commands (I have kept the clock, IO, UART and CTU config and the state machine).

I have created a new recorder in Freemaster 2.0, but everytime I am trying to start it I am getting a response timeout error when the trigger condition is true.

eusebiu_bivol_0-1612610435264.png

I am able to see and modify the variables in the Watch window.

eusebiu_bivol_1-1612610498199.png

Do you have any idea why the recorder is not working?
Thank you!

 

0 项奖励
回复
1 解答
1,156 次查看
eusebiu_bivol
Contributor II

The problem is solved.

My mistake was that I was trying to use the recorder while I was in debug mode with S32DS.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,157 次查看
eusebiu_bivol
Contributor II

The problem is solved.

My mistake was that I was trying to use the recorder while I was in debug mode with S32DS.

0 项奖励
回复