I´m trying to use USBDM with MC56F8006. Inside CW 8.3 it works, but the stand alone MC56F Programmer software is not working. Ex., trying to Mass Erase the dsc, always returns the message "Execution of TCL script returned an error".
Somebody can help ? It is USBDM-JMxx-CF-0001.
Dear Xiangjun Rong;
CW 8.3 supports the USBDM, see photo, and is
running well.
The problem is with version _200 of USBDM, the older
version _140 runs.
BR,
Paulo R L Barbosa
Nova PRecursor
Industria,
Comércio e Serviços
27 Anos 1990-2017
Av João Carlos da Silva Borges
873 Sala 2
04726-001 São Paulo SP
(11)2337-1591
Skype NovaPRecursor
Em
04.08.2017 02:33, xiangjun.rong escreveu:
NXP COMMUNITY
RE:
USBDM IS NOT RUNNING WITH MC56F
reply from xiangjun.rong in
Digital Signal Controllers - View the full discussion
>