Hi,
Currently have a project with a MC56F84763 that when I run my project through the debugger after I download it using CW 10.6 and a multilink universal the code runs fine. If I remove the debugger and hope that the code would start and run on it's own it does not seem to run and I am looking for my outputs and none are changing. Is there a setting in the project that I am not seeing? I have made changes to my kinetis release projects to make them work and wondering if there are similar tweaks that I do not see in DSC projects.
Thanks,
Lee
If it starts up correctly in debug mode, but not in stand-alone mode, the possible reason may be:
1) Watchdog reset. Is the watchdog being serviced? Please first disable the watchdog in your application and test whether it makes any difference.
2) Incorrect interrupt vector. In debug mode, the program starts from Entry Point which is set in the Target setting. While in stand-alone mode, it starts from vector table.
Please check whether the vector table is placed at the correct address in program flash. And the reset vector is correctly calling the start up routine.
3) Lost data in RAM. Please check the linker command file and MAP file, whether there’s code or initialized data are placed in RAM, please place them in flash.
4) Initialized global variable, whether they are initialized correctly. This is another difference between running in debug mode and stand-alone mode. When program before debugging, CodeWarrior will erase the memory before writing, but in stand-alone mode.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is the board electrically dependent on the JTAG connection to the computer?
What kind if board is it running on?
Is the watchdog being serviced?
Best Regards,
John L. Winters
Senior Applications Engineer
AMR/EU MCU & MPU AE Group
Freescale Inc.
2100 Elliot Road
This email and any associated attachments have been classified as:
Freescale Confidential and Proprietary