DSC56800EX Quick start Version 2.6.31.0 Crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DSC56800EX Quick start Version 2.6.31.0 Crash

跳至解决方案
1,660 次查看
antonio66
Contributor III

Hi,

 

I'm using the Quick start for MC56F82323 release 2.6.31.0

If i try to do the setup on the "QT_A0-Counter_0"  on the  "secondary input"   "Counter #3 input pin"

the system crash like the attached image.

Solutions ?

by

 

 

75125_75125.pngpastedImage_0.png

标签 (1)
0 项奖励
回复
1 解答
1,509 次查看
TICS_Fiona
NXP Employee
NXP Employee

Sorry for the waiting. I got the solution from the developers.

Attached file is fix of this issue.

You can apply the fix by copy this file into C:\Freescale\DSC56800EX_Quick_Start_r2.6\tools\gct\ folder

Fix removes option to select input pin 3, because pin is not in this package.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,510 次查看
TICS_Fiona
NXP Employee
NXP Employee

Sorry for the waiting. I got the solution from the developers.

Attached file is fix of this issue.

You can apply the fix by copy this file into C:\Freescale\DSC56800EX_Quick_Start_r2.6\tools\gct\ folder

Fix removes option to select input pin 3, because pin is not in this package.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,509 次查看
antonio66
Contributor III

Hi Mr. Xin Kuang,

The cpu is the MC56F82323 thank.

best regards.

0 项奖励
回复
1,509 次查看
TICS_Fiona
NXP Employee
NXP Employee

I reproduced the problem with CodeWarrior v10.6.5 and DSC56800EX Quick Start v2.6.31. I have contacted the developers for this issue, and will reply again as soon as I get any progress on it.  In addition, I created a SR#1-4061015762 for you to trace this problem.

Fiona Kuang

Technical Information & Commercial Support

0 项奖励
回复