Bootloader utility for MC56F83xxx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootloader utility for MC56F83xxx

Bootloader utility for MC56F83xxx

The MC56F83xxx is the latest DSC family, it integrates new features such as CAN-FD, USB, enhanced DMA, can be used in motor control, switch mode power supply applications.

The MC56F83xxx runs code in on-chip flash, so the Bootloader’s main task is to update the internal flash memory with an embedded application firmware image during manufacturing, or at any time during the life of the device. The Bootloader does the provisioning by acting as a slave device, and listening to various peripheral ports where a master can start communication.

The Doc describes the procedures to use the bootloader to download application code to flash, for example the hardware connection, generating S-Record file, selecting the S-Record file, the blhost commands, especially, the traps customer may face.

标签 (1)
标记 (2)
附件
无评分
版本历史
最后更新:
‎07-24-2020 01:30 AM
更新人: