In MC56F83783 how to configure ADC in polling method. Is there any application note available for ADC configuration.
Hi,
There is SDK package for MC56F83xxx, pls download it from the link:
https://mcuxpresso.nxp.com/en/welcome
For the ADC, there are three examples:
All of then is based in interrupt mode, if you want to use polling mode, you can use any one of the 4 examples, and disable interrupt, then the use the following code to implement the polling mode:
.................
while(1)
{
1)start ADC convertion
2)while(ADC_STAT&1<<11) {} //polling EOSI0 bit
3)reading ADC result register to memory
}
Pls try to modify the example code
We have not the application note about ADC polling mode
Hope it is helpful
BR
Xiangjun Rong