Micron® Technology: Micron’s Memory Solutions for the New i.MX 8 Microprocessor Family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Micron® Technology: Micron’s Memory Solutions for the New i.MX 8 Microprocessor Family

Micron® Technology: Micron’s Memory Solutions for the New i.MX 8 Microprocessor Family

During this session, we will discuss the new memories supported on the new i.MX8 processor family. For DRAM, this will include DDR4 and Low Power DDR4 (LPDDR4). For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. This year, we will provide additional information on LPDDR4X (X=lower power I/O) as well as eMMC 5.1 high performance features including command queueing, and several new Cache operations. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems.  

添付
評価なし
バージョン履歴
最終更新日:
‎06-18-2018 05:54 PM
更新者: