Hello,
The .inf file (see atachment) that I usually use in Windows 7 (32 AND 64 bits) to install Virtual Com Port when I plugged MC9S08JM60 or MCF51JM128 with Freescale USB CDC Stack is refused under Windows 8.
Does someone can help me to modify this file ?
Or could you give me a file that work ?
I found nothing about this issue in freescale webpages...
Many thanks,
Thomas.
Original Attachment has been moved to: Freescale-CDC_driver_x86_x64.inf.zip
If you want your CDC device to work in any Windows 8 Machine (32 and 64) without need of drivers or .inf files you can set your stack VID to 04D8 and PID to 000A and your device will be recognized as Serial Port automatically, windows 8 has built-in drivers (which is in reality the same drivers used by the inf files posted in this thread that are made by Microsoft) associated to this VID/PID pair. The downside is that in the Hardware manager the manufacturer will show as "Microchip Technology, Inc.". I know it's a nuisance to show a Freescale device as a Microchip but somehow Microchip managed to make Microsoft ship a .inf file with windows 8 to recognize their devices automatically and other manufacturers didn't.
Attached is a tweaked self-signed driver that worked for me, its purpose is to allow you to load the driver without first "disabling driver signature checking" on Windows 8. It is self-signed, so it will give you a warning that the cert cannot be verified.
If you would like some more detail, here is a link to instructions on how to do it:
Test Signing (Windows Drivers)
NOTE TO FREESCALE: please sign your driver with a legitimate signature. It isn't that involved, doesn't take very long to do OR test, and would clean up these issues.
This is the OFFICIAL Freescale answer :
From: "Freescale Support" <support@freescale.com>
Sent: Wednesday, November 07, 2012 7:56 PM
Subject: RE: SR# 1-963808141 : Windows 8 USB CDC Setup (or .inf) file ?
In reply to your Service Request SR 1-963808141:
I’m afraid that there is not available an INF file with Windows 8 support
yet. It may be probably included on future releases of Freescale USB stack
(which includes the CDC example).
Please accept our apologies for any inconveniences this may cause. Have a
nice day.
Thank you for your interest in Freescale Semiconductor products and for the
opportunity to serve you.
Should you need to contact us with regard to this message, please see the
notes below.
Best Regards,
Carlos Jose
Technical Support
Freescale Semiconductor
SO WAIT AND SEE...
This is because of Windows 8 blocking the installation of unsigned drivers. There's a workaround, but it's a bit of a pain: