MCF52277RM - 4 wire resistive touch panel interface.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52277RM - 4 wire resistive touch panel interface.

474 次查看
anujtopiwala
Contributor I

Using MCF52277RM I need to establish 4 wire resistive touch panel interface. But I have 6-8 inch cable extending from the touch panel to main board. Will the inbuilt Touch controller with ADC biasing circuit be enough for noise free interface. The touch panel resistance is 200 ~900 ohm both x and y side with < 1.5 % linearity.

标签 (1)
0 项奖励
回复
0 回复数