Before my brain melts, can anyone clarify the port/pin registers for this?
As far as I can make out:
FB_D0 = PTH6 = Pin51
FB_D1 = PTH7 = Pin50
FB_D2 = PTH0 = Pin47
FB_D3 = PTH1 = Pin46
FB_D4 = PTH2 = Pin1
FB_D5 = PTH3 = Pin140
FB_D6 = PTH4 = Pin139
FB_D7 = PTH5 = Pin138
And the config registers are organised in differing orders:
MCF_GPIO_PTHPAR_ is in FB_Dx order where FB_D0 is BIT0&1 and FB_D7 is BIT14&15
MCF_GPIO_DDRTH_ is in PTHx order where DDRTH0 is BIT0 and DDRTH7 is BIT7
MCF_GPIO_SETTH_ is in PTHx order where SETTH0 is BIT0 and SETTH7 is BIT7
MCF_GPIO_CLRTH_ is in PTHx order where CLRTH0 is BIT0 and CLRTH7 is BIT7
So the question is, say I want to set pin 138 as an output and toggle it, do I set PTHPAR7 = GPIO to assign it but then set DDRTH5 to make it an output, and write MCF_GPIO_PORTTH ^= MCF_GPIO_PORTTH_PORTTH5 to toggle it.
解決済! 解決策の投稿を見る。
This issue has come back to bite me again, the MCF52259 reference manual states that PORTTH is at IPSBAR+0x10_0003 (well, it actually states it's "POTRTH" as someone seems to have had a bad day with the spelling
However, as I am trying to read the pins as inputs the manual states I should read the pin data/set data register PORTnP/SETn which it then calls PORTTH/SETTH, with an address of IPSBAR+0x10_0033
The pin data/set data register "SetTF" is indeed defined at IPSBAR+0x10_0033, but if you read MCF_GPIO_PORTTH you are reading the data output register and in fact need to (counter-intuitively) read the MCF_GPIO_SETTH register.
IJust thought I'd tag this on the end in case someone else finds it useful.
A bit more fiddling today has found that the registers are assigned relative to PORTTH, so if I want to set pin 138 as an output and toggle it, I set PTHPAR5 = GPIO to assign it and set DDRTH5 to make it an output, and write MCF_GPIO_PORTTH ^= MCF_GPIO_PORTTH_PORTTH5 to toggle it.
However, the header files for the micro seem to be the wrong way round. PTH2 & 3 (FB4 & 5) are I2C ports, yet the bit field for the port includes:
MCF_GPIO_PTHPAR_MB_D5_SCL1 (0x800) which sets PTH5 to its secondary function as CANRX.
Confused yet?
This issue has come back to bite me again, the MCF52259 reference manual states that PORTTH is at IPSBAR+0x10_0003 (well, it actually states it's "POTRTH" as someone seems to have had a bad day with the spelling
However, as I am trying to read the pins as inputs the manual states I should read the pin data/set data register PORTnP/SETn which it then calls PORTTH/SETTH, with an address of IPSBAR+0x10_0033
The pin data/set data register "SetTF" is indeed defined at IPSBAR+0x10_0033, but if you read MCF_GPIO_PORTTH you are reading the data output register and in fact need to (counter-intuitively) read the MCF_GPIO_SETTH register.
IJust thought I'd tag this on the end in case someone else finds it useful.