DATA SHEET FOR FREESSCALE HCS12 T-BOARD MICROCONTROLLER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DATA SHEET FOR FREESSCALE HCS12 T-BOARD MICROCONTROLLER

1,178 次查看
gonzalo_laradel
Contributor I

Hi everyone,

I'm a user of a 68HC12 microcontroller. My board is one made by the formerly Freescale Semicondauctors but I;m having trouble finding the right data sheet for it. The data sheets in NXP don't talk about TC2 which is the register use to store the value the binary counter must be equal to perform output compare. Also, the Timer Channel registers are 7 bits wide whereas in the Freescale data sheet, it is 16 bits wide. I'm not sure which of the variants corresponds to the microcontroller I have. The product No. of the microcontroller I'm using is MC9S12DP512 CVPE 4L00M QQJU1106 but the MC9S12DP512, supposedly, corresponds to another family of microcontrollers. I am getting really confused and any help would be really appreciated. Thank you.

Kind Regards,

Gonzalo Lara de Leyva

P.D. I attach the chapter on timers for the original datasheet. I only have this chapter but not the full data sheet.

标签 (1)
标记 (1)
1 回复

1,004 次查看
TomE
Specialist II

You've typed "MC9S12DP512CVPE", but I suspect you mean "MC9S12DP512CPVE":

MC9S12DP512CPVE Product Information|NXP 

.

All the Reference Manuals are on the above page under "Documentation".

Also, this is the "Coldfire" forum. You should MOVE your post to the one specific for the MC9S12, which is here:

https://community.nxp.com/community/s32/16-bit 

There's an option to move your post somewhere under one of the "Edit" options.

Tom