When the AN3470/AN3518 (TCP/IP Lite based application notes) are compiled with CW7.0, compilation fails.
TCP/IP Lite can be downloaded from the Freescale web site by itself too, not as part of an application note. This version is more recent than the one in the application note and does compile fine with CW7.0.
This made me decide to port my AN3518-based application to this more recent version of TCP/IP Lite. It compiles fine with CW7.0 but... for some reason the application doesn't run. I haven't figured out why, I decided that since it works fine when compiled with CW6.4, I will simply keep using CW6.4. CW6.4 requires a lot less hard disk space also! (not that this matters these days...)
I also read somewhere in the TCP/IP Lite documentation :
ColdFire TCP/IP Lite Project Version 2.0 October 12, 2007
CodeWarrior for ColdFire currently has a stable release with Version 6.4. A Version 7.0 is expected in December 2007 and a new drop of this project will be released then. This is why we have included 6.4 in the filename.
So I guess one day a CW7.0 compatible version of TCP/IP Lite should arrive...