what codewarrior suite should I purchase?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what codewarrior suite should I purchase?

2,166 Views
bbjh1
Contributor I

Hi,

 

I am trying to buy a codewarrior suite so that I can get rid of the license issues that always appear in my projects. I was wondeirng if someone can help me and give me the main difference between the two suites (basic and professional). I don't think I need the professional suite but I am not really sure.

Thank you.

Labels (1)
0 Kudos
Reply
4 Replies

707 Views
martinw
Contributor III

If you are running Linux on your board then the basic does the job.

 

If you want to write embedded code without an OS you need the professional version of CodeWarrior MobileGT.

 

Both can be hosted on either windows or linux.

 

Cheers


Martin

 

0 Kudos
Reply

707 Views
bbjh1
Contributor I

Hey Martin, thank you for you quick reply. I am using the mpc5121e processor on the ADS5121 board, so you think that the basic suite is enough?

 

Thx again.

0 Kudos
Reply

707 Views
martinw
Contributor III

Are you using linux on the target?  If so then I believe the basic will be ok, although I've never used it.

 

If you are not using linux on the target then you need the Pro version.  That's what we use on the MPC5121 as we write code which does not have an OS.

 

Best thing is to download a demo of the basic suite which will run for a period of time (30 days i think) and try it to make sure it does everything you want.

 

 

0 Kudos
Reply

707 Views
CrasyCat
Specialist III

Hello

 

A CodeWarrior Basic edition will only allow you to program flash and run hardware diagnostic tools.

You will not be able to build or debug any bare board application.

 

If you are planning to do develop and debug Linux applications (i.e. develop application on top of a Linux kernel running o the HW board) the basic edition is enough as well.

But keep in mind that you will not be able to do any Linux kernel debugging. 

 

CrasyCat

0 Kudos
Reply