tblcf_gdi.dll  don't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tblcf_gdi.dll  don't work

Jump to solution
1,890 Views
zipper
Contributor I

I use the CodeWarrior 7.2 and use the tblcf_gdi.dll.When I debugged,an error occured.
 The Attachment shows the error.Who can help me?Thanks very much.

Labels (1)
0 Kudos
Reply
1 Solution
1,597 Views
sergio29
Contributor II

:smileyhappy:

Hi,

Read and respect then "CodeWarrior setup" of this document

See attached file

Sergio

 

View solution in original post

0 Kudos
Reply
13 Replies
1,598 Views
sergio29
Contributor II

:smileyhappy:

Hi,

Read and respect then "CodeWarrior setup" of this document

See attached file

Sergio

 

0 Kudos
Reply
1,597 Views
zipper
Contributor I

Do you have the proper driver for the JB16 based TBLCF for CFV2 in CW7.2?

0 Kudos
Reply
1,597 Views
sergio29
Contributor II

 

Hi

As explained in CodeWarrior setup in "Edit" "Preferences" "Remote Connection" ,  your named

TBLCF Connection have to point to tblcf_gdi.dll and not to USBDM_GDI_CFVx.dll by cliking on "Change" and browsing 

to your tblcf_gdi.dll in the correct repertory.

Your attached file show CW7.2 looking for USBDM_GDI_CFVx.dll instead of tblcf_gdi.dll.

It works perfectly for me with JB16 TBLCF

 

0 Kudos
Reply
1,597 Views
zipper
Contributor I
0 Kudos
Reply
1,597 Views
sergio29
Contributor II

Voici tout

0 Kudos
Reply
1,597 Views
sergio2985
Contributor I

 

 

With CW7.2, there is no TBLCF repertory under \Program Files\Freescale\CodeWarrior for ColdFire V7.2\bin\Plugins\Support\ColdFire

 

Freescale supplies  only Abatron, OSBDM and PEMicro repertories.

 

Where have you found all your TBLCF files ?

 

 

 

0 Kudos
Reply
1,597 Views
zipper
Contributor I

Then what's the version of CW that you are using for coldfire V2?

0 Kudos
Reply
1,597 Views
sergio2985
Contributor I

Hi

 

I'm using TBLCF for Coldfire V2 MCF52236 and MCF5271 with  CW7.1 or CW7.2 with success

0 Kudos
Reply
1,597 Views
zipper
Contributor I

I am wrong.Now I know those files are not tblcf files.They are for TBDML,not for JB16 based TBLCF.

 

Bestregards

zipper

0 Kudos
Reply
1,597 Views
zipper
Contributor I

I made a folder named tblcf.Maybe tblcf does not work in CW7.2.I will try it in CW7.1.Thank you very much.

 

Bestregards 

 

zipper

0 Kudos
Reply
1,597 Views
zipper
Contributor I

Hi,I did as what you said,but it still won't work.I found a lot of dlls and none could work properly.I think my driver for the TBLCF may not be corrretly installed.Do you have the driver for TBLCF?I can't find other driver on the Internet.

 

Bestregards

zipper

0 Kudos
Reply
1,597 Views
zipper
Contributor I

:smileywink: Do you have the proper driver for the JB16 based TBLCF for CFV2 in CW7.2?

0 Kudos
Reply
1,597 Views
zipper
Contributor I

Hi,my device is TBLCF that is based on JB16 for CFV2,I got a driver and installed it.But the CW7.2 can't dectect it.
 

0 Kudos
Reply