To use gdb via the codewarrior tap with the LS1046ARDB some gdb monitor commands are needed according to the example video for previous (refence design) boards. I can connect to the gdb proxy on the codewarrior tap, but to connect to the board, the jtag chain must be known/configured:
(gdb) mon jtag_chain
Chain not configured
Not connected to target
(gdb) mon connect
Connected to CCS
Connected to probe fpga
Unknown target
Protocol error with Rcmd
As these monitor command are extensions to the normal gdb and nxp specific, I need to know how to configure gdb to be able to connect to the target. Do you have ls1046ardb_init.gdb file? Can you at least provide the required information/commands need to connect to the target via the gdbproxy on the codewarrior tap.
Look at the following:
http://www.nxp.com/video/board-level-bringup-using-codewarrior-tap-and-gdb:BOARDLVL_CWTAPGDB_VID
It is too old demo project. This demo project is closed now.
Create please technical case if additional information is needed.
See the following:
https://community.nxp.com/thread/381898
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------