codewarrior 10.5 for pa , connect chip, invalid sequence number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

codewarrior 10.5 for pa , connect chip, invalid sequence number

908件の閲覧回数
ybhao
Contributor I

111.png222.png333.png

 

444.png

 

i use codewarrior tap connect p2020 ,  before it connect ok.  

now i install IDE at NEW computer ,  but license is ok now.

when i connect chip, i get invalid sequence number err, thank you .

 

0 件の賞賛
返信
2 返答(返信)

899件の閲覧回数
ybhao
Contributor I

ok, this problem is solved, ccs should detect cwtap, then is ok

bin) 2 % findcc cwtaps
FSL0565B2 (00:04:9f:05:65:b2): CodeWarrior TAP (3.3V)
Power Architecture JTAG/COP Probe Tip
Boot Loader v1.0.1
Operating System v1.0.4
(bin) 2 %

but now i have another bug,666.png

ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 10
Error message: Connection refused
ccs_open
ipaddr = 127.0.0.1
port = 41475
timeout = 15
serverh = 0
ccs_open; ccs_error = 0
ccs_get_connection_count
serverh = 0
count = 1
ccs_get_connection_count; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 0
ccs_available_connections
serverh = 0
count = 0
ccs_available_connections; ccs_error = 0
ccs_config_cc
serverh = 0
config_string = cwtap:0
ccs_config_cc; ccs_error = 0
ccs_available_connections
serverh = 0
count = 1
ccs_available_connections; ccs_error = 0
ccs_cc_version
serverh = 0
cc = 0
version.major = 0
version.minor = 0
ccs_cc_version; ccs_error = 0
ccs_set_timeout
serverh = 0
timeout = 15
ccs_set_timeout; ccs_error = 0
ccs_available_connections
serverh = 0
count = 1
ccs_available_connections; ccs_error = 0
ccs_config_server
serverh = 0
cc = 0
server_config = 0
value = 12500
ccs_config_server; ccs_error = 0
ccs_get_config_chain
serverh = 0
device_list: (size = 0)
ccs_get_config_chain; ccs_error = 0
ccs_config_chain
serverh = 0
cc = 0
device_list: (size = 1)
device[0]:: core_type=mpc8572(102)
ccs_config_chain; ccs_error = 0
ccs_get_config_chain
serverh = 0
device_list: (size = 3)
ccs_get_config_chain; ccs_error = 0
ccs_get_config_chain
serverh = 0
device_list: (size = 3)
device[0]:: core_type=mpc8572(102)
device[1]:: core_type=Draco/m HIP8(53)
device[2]:: core_type=Draco/m HIP8(53)
ccs_get_config_chain; ccs_error = 0
ccs_send_message
coreh = [serverh:0;cc_index:0;chain_pos:1]
message = 3
ccs_send_message; ccs_error = 0
ccs_stop_core
coreh = [serverh:0;cc_index:0;chain_pos:1]
ccs_stop_core; ccs_error = 0
ccs_read_register
coreh = [serverh:0;cc_index:0;chain_pos:1]
index = 287
count = 1
size = 4
value: (size = 4)
80211051
ccs_read_register; ccs_error = 0; duration=3 ms
ccs_run_core
coreh = [serverh:0;cc_index:0;chain_pos:1]
ccs_run_core; ccs_error = 0
ccs_reset_to_mixed
chain_pos: (size = 3) { 0 (halt) 1 (halt) 2 (halt) }
ccs_reset_to_mixed; ccs_error = 39; duration=2809 ms
Error message: Draco/m HIP8: ELF is not in expected HALT mode
ccs_get_subcore_error
serverh = 0
cc = 0
error = -2147483635
chain_pos = 1
ccs_get_subcore_error; ccs_error = 0; duration=2 ms
ccs_available_connections
serverh = 0
count = 1
ccs_available_connections; ccs_error = 0
ccs_delete_cc
serverh = 0
count = 0
ccs_delete_cc; ccs_error = 0
ccs_kill_server
serverh = 0
ccs_kill_server; ccs_error = 0

0 件の賞賛
返信

894件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to page 6 and 7 in the attachment.

•Ensure HRESET not tied to TRST

•HRESET to the processor exclusive to COP/JTAG header

0 件の賞賛
返信