Unable to recover NOR Flash on T4240RDB Rev 2.0 With CW-10.5.1 and RCW (Jtag Chain) Override method

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to recover NOR Flash on T4240RDB Rev 2.0 With CW-10.5.1 and RCW (Jtag Chain) Override method

2,590 Views
hemanthkv
Contributor I

Unable to recover NOR flash for T4240rdb with CodeWarrior 10.5.1 with Host System Ubuntu 14.04.5.

Using Codewarrior USB TAP and the flash programmer to flash a NOR flash image to my t4240rdb board

 

Getting following error "Failed to correctly configure the JTAG chain(CCSProtocalPlugin)"

173295_173295.pngFlash-programmer-error.png

 

Created BareBoard Project and used T4240RDB_init_sram.tcl as initialization file and chosen CodeWarrior USB TAP to be the connection type(Both when creating the project or change the settings after creating are OK).

For overriding RCW  used T4240RDB_RCW...-rev2.0.txt in the JTAG file configuration panel.

173296_173296.pngUSB-Tap-HW.png

 

Attached is ccs logs

 

173297_173297.pngCCS.png

 

Request for help in recovering board by properly flashing NOR flash with help of Code Warrior.

 

Labels (1)
0 Kudos
26 Replies

1,355 Views
hemanthkv
Contributor I

Request for help on proceeding further.

Thanks.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

The RCW override is not working, unless the latest CPLD image is used. To get the latest CPLD image you should contact your NXP representative. 

If you want to recover the RCW in EEPROM, you can fallow the steps below:

- In a linux environmental write the sdcard uboot to a SD card

- Insert SD card into T4RDB board and set SW3[4]=0 and SW2[1]=1 to boot uboot

- In Uboot, load the RCW image to ram then write it to EEPROM using i2c write <load_addr> 50 .01 78

- Set SW3[4]=0 and reset

Adrian

0 Kudos

1,355 Views
hemanthkv
Contributor I

Hello Adrian,

Presently we don't have sd_card slot working.

If we cant recover with RCW override then do we have any other way of recovering the board.

Thanks,

Hemanth.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

Please contact your NXP representative and a new CPLD image can be provided. The latest CPLD image allow RCW source from NOR.

0 Kudos

1,355 Views
hemanthkv
Contributor I

Hello Adrian,

I have received latest pof file from NXP representative which will support RCW override.

Request the procedure for flashing this pof file.

Can we use code-warrior with USB tap connection or do we need to use Usb-blaster?

Thanks,

Hemanth.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

Updating the pof file is not possible using CodeWarrior/USB tap. Internally, we used some programmer from Altera (Quartus).

Adrian 

0 Kudos

1,355 Views
hemanthkv
Contributor I

Hello Adrian,

Updated pof file with Altera (Quartus) Programmer which  was successful.

But RCW override is failing.Following is ccs log

verbose logging

ccs log
CCSAPI connection #1 accepted from localhost at Mon Jan 16 20:46:24 2017
check_min_version(serverh=0,*version)
  api version: 00000004 00000006
get_connection_count(serverh=0,cc_index=0,*count)
  count:1
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
available_connections(serverh=0,*count,*cc)
  connections:
get_connection_count(serverh=0,cc_index=0,*count)
  count:1
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
available_connections(serverh=0,*count,*cc)
  connections:
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
delete_cc(serverh=0,cc=0)
setup_cc(serverh=0,config_string= utap:0 )
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
cc_version(serverh=0,cc_index=0,index=-240214688,*version)
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
available_connections(serverh=0,*count,*cc)
  connections: {0,70,0x00000000}
config_server(config_reg=0,config_data=0x000027F6)
get_config_chain(serverh=0,cc=0)
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
  devlist: t4amp
config_template(coreh.{serverh=0,cc_index=0,chain_pos=0},config_reg=2,config_data=0x00000001)
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210001,size=4,*reg)
  reg: 16070019
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210002,size=4,*reg)
  reg: 18101916
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210003,size=4,*reg)
  reg: 00000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210004,size=4,*reg)
  reg: 00000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210005,size=4,*reg)
  reg: 70701050
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210006,size=4,*reg)
  reg: 00448C00
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210007,size=4,*reg)
  reg: 0C020000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210008,size=4,*reg)
  reg: F5000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210009,size=4,*reg)
  reg: 00000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210010,size=4,*reg)
  reg: EE0000EE
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210011,size=4,*reg)
  reg: 00000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210012,size=4,*reg)
  reg: 000287FC
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210013,size=4,*reg)
  reg: 00000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210014,size=4,*reg)
  reg: 50000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210015,size=4,*reg)
  reg: 00000000
write_register(coreh.{serverh=0,cc_index=0,chain_pos=0},index=210016,size=4,*reg)
  reg: 00000028
reset_to_debug(serverh=0,cc=0)
  ERROR(39): Subcore error encountered during multicore operation
parse_error_ext(coreh.{serverh=0,cc_index=0,chain_pos=0}, 39)
  error: T4240: Scan timeout
get_subcore_error(serverh=0,cc=0,*error,*chain_pos)
  error: Scan timeout
  chain_pos: 0
reset_to_debug(serverh=0,cc=0)
  ERROR(39): Subcore error encountered during multicore operation
parse_error_ext(coreh.{serverh=0,cc_index=0,chain_pos=0}, 39)
  error: T4240: Scan timeout
get_subcore_error(serverh=0,cc=0,*error,*chain_pos)
  error: Scan timeout
  chain_pos: 0
reset_to_debug(serverh=0,cc=0)
  ERROR(39): Subcore error encountered during multicore operation
parse_error_ext(coreh.{serverh=0,cc_index=0,chain_pos=0}, 39)
  error: T4240: Scan timeout
get_subcore_error(serverh=0,cc=0,*error,*chain_pos)
  error: Scan timeout
  chain_pos: 0
CCSAPI connection #1 from localhost closed at Mon Jan 16 20:46:40 2017

Thanks,

Hemanth.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

Please confirm your cpld image is T4240RDB_V7p0.pof (T4240RDB_2016_0602_0933).

Adrian

0 Kudos

1,355 Views
hemanthkv
Contributor I

Hello Adrian,

The cpld Image which I received and flashed is T4240RDB_V7p0.pof(Release notes mentions T4240RDB_2016_0602_0933).

Thanks,

Hemanth.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

Take the script attached and run it in ccs using:

(bin) 56 % source C:/CCS_RCW_override_t4240rdb.tcl

My test board is set for NOR boot:

SW2: ON ON OFF OFF

SW3: OFF OFF OFF ON

SW4: ON ON ON ON

SW1: ON ON ON ON

ccs should report no error when running the script. I tested on my side and RCW override is working fine with the new cpld image.

Adrian 

0 Kudos

1,355 Views
hemanthkv
Contributor I

Hello Adrian,

You mean switch setting like below.In previous reply you have started from SW2 to SW5

SW1: ON ON OFF OFF

SW2: OFF OFF OFF ON

SW3: ON ON ON ON

SW4: ON ON ON ON.

After setting above switch setting running the script shared resulted in following

Script log
0: USB TAP (JTAG) (utap) CC software ver. {1.3}
Chain Position 0: T4AMP SoC
Chain Position 1: e6500 thread 0
Chain Position 2: e6500 thread 1
Chain Position 3: e6500 thread 0
Chain Position 4: e6500 thread 1
Chain Position 5: e6500 thread 0
Chain Position 6: e6500 thread 1
Chain Position 7: e6500 thread 0
Chain Position 8: e6500 thread 1
Chain Position 9: e6500 thread 0
Chain Position 10: e6500 thread 1
Chain Position 11: e6500 thread 0
Chain Position 12: e6500 thread 1
Chain Position 13: e6500 thread 0
Chain Position 14: e6500 thread 1
Chain Position 15: e6500 thread 0
Chain Position 16: e6500 thread 1
Chain Position 17: e6500 thread 0
Chain Position 18: e6500 thread 1
Chain Position 19: e6500 thread 0
Chain Position 20: e6500 thread 1
Chain Position 21: e6500 thread 0
Chain Position 22: e6500 thread 1
Chain Position 23: e6500 thread 0
Chain Position 24: e6500 thread 1
T4AMP SoC: Scan timeout

Thanks,

Hemanth.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

Just correct my previous post. The SW settings I'm using:

SW2: ON ON OFF OFF

SW3: OFF OFF OFF ON

SW4: ON ON ON ON

SW1: ON ON ON ON

Adrian

0 Kudos

1,354 Views
hemanthkv
Contributor I

Hello Adrian,

Getting "T4AMP SoC: Scan timeout" with Switch settings specified.

SW2: ON ON OFF OFF

SW3: OFF OFF OFF ON

SW4: ON ON ON ON

SW1: ON ON ON ON

Header 1

bin) 6 % source /home/tester/CCS_RCW_override_t4240rdb.tcl
0: USB TAP (JTAG) (utap) CC software ver. {1.3}
Chain Position 0: T4AMP SoC
Chain Position 1: e6500 thread 0
Chain Position 2: e6500 thread 1
Chain Position 3: e6500 thread 0
Chain Position 4: e6500 thread 1
Chain Position 5: e6500 thread 0
Chain Position 6: e6500 thread 1
Chain Position 7: e6500 thread 0
Chain Position 8: e6500 thread 1
Chain Position 9: e6500 thread 0
Chain Position 10: e6500 thread 1
Chain Position 11: e6500 thread 0
Chain Position 12: e6500 thread 1
Chain Position 13: e6500 thread 0
Chain Position 14: e6500 thread 1
Chain Position 15: e6500 thread 0
Chain Position 16: e6500 thread 1

T4AMP SoC: Scan timeout

Thanks,

Hemanth.

0 Kudos

1,354 Views
addiyi
NXP Employee
NXP Employee

In the previous SW settings I miss the SYSCLK setting. So please use the following:

 

SW2: ON ON OFF OFF

SW3: OFF OFF OFF ON

SW4: ON ON ON ON

SW1: ON ON OFF OFF

Adrian

0 Kudos

1,354 Views
hemanthkv
Contributor I

Still facing "Scan Timeout" ,even after modifying switch settings specified as

SW2: ON ON OFF OFF

SW3: OFF OFF OFF ON

SW4: ON ON ON ON

SW1: ON ON OFF OFF

Following is the log

(bin) 20 % source /home/Downloads/CCS_RCW_override_t4240rdb.tcl
0: USB TAP (JTAG) (utap) CC software ver. {1.3}
Chain Position 0: T4AMP SoC
Chain Position 1: e6500 thread 0
Chain Position 2: e6500 thread 1
Chain Position 3: e6500 thread 0
Chain Position 4: e6500 thread 1
Chain Position 5: e6500 thread 0
Chain Position 6: e6500 thread 1
Chain Position 7: e6500 thread 0
Chain Position 8: e6500 thread 1
Chain Position 9: e6500 thread 0
Chain Position 10: e6500 thread 1
Chain Position 11: e6500 thread 0
Chain Position 12: e6500 thread 1
Chain Position 13: e6500 thread 0
Chain Position 14: e6500 thread 1
Chain Position 15: e6500 thread 0
Chain Position 16: e6500 thread 1
T4AMP SoC: Scan timeout

Thanks,

Hemanth.

0 Kudos

1,354 Views
addiyi
NXP Employee
NXP Employee

You could try different selection for SYSCLK and DDRCLK, maybe the core will respond.

0000 66.67 66.67

0001 66.67 100

0010 66.67 125

0011 (Default) 66.67 133.33

0100 100 66.67

0101 100 100

0110 100 125

0111 100 133.33

1000 125 66.67

1001 125 100

1010 125 125

1011 125 133.33

1100 133.33 66.67

1101 133.33 100

1110 133.33 125

1111 133.33 133.33 

If this is not working, my guess is the board have some hardware issues.

Adrian

0 Kudos

1,354 Views
hemanthkv
Contributor I

For all the above switch setting got "T4AMP SoC: Scan timeout" on running CCS_RCW_override_t4240rdb.tcl in ccs.

Thanks,

Hemanth.

0 Kudos

1,354 Views
addiyi
NXP Employee
NXP Employee

On my side it works ok using the below two cases:

1. Board set to hardcoded rcw, with not using the write_reg in the tcl script

SW1: OFF OFF ON ON

SW2: ON OFF OFF OFF

SW3: OFF OFF OFF OFF

SW4: OFF OFF OFF OFF

2. Board set to boot for NOR, with write_reg in the tcl script

SW1: OFF OFF ON ON

SW2: ON ON OFF OFF

SW3: OFF OFF OFF OFF

SW4: OFF OFF OFF OFF

For both above cases, ccs is not returning "Scan timeout"

Adrian

0 Kudos

1,355 Views
hemanthkv
Contributor I

Hello Adrian,

Switch setting are as specified in T4240RDB_aeabi_README.txt (\PA\PA_Support\Readme\QorIQ_T4\). 

switch setting
NOR_BOOT:
---------

 SW1 : 0x3 = 1100     SW2 : 0xF = 1111     SW3 : 0xF = 1111    SW4 : 0xF = 1111
 

Note: ON side is 0, the other side is 1.

Thanks,

Hemanth.

0 Kudos

1,355 Views
addiyi
NXP Employee
NXP Employee

Depending on CPLD image RCW override is not supportted. Try using hardcoded from dip switches. For that set SW2[1:2] = 01 and SW3[4] = 1, where 0 is ON and 1 is OFF.

Adrian

0 Kudos