I tried a simple exercise, import an existing RCW in QCVS4.4.1 and regenerate it.
Unfortunately, the new RCW is different in a few places and the target fails to boot.
Except for the checksum, the only difference is the following bytes:
005a 0421 -> 0050 0401
From what I understand, these bytes are reserved so I have no ways to know what they are doing.
Original RCW (boots at addr 0x60000000)
=> md.w 62800000
62800000: 55aa 55aa ee01 0001 0806 0a00 0000 0000 .U.U............
62800010: 0000 0000 0000 0000 0070 0000 0000 0079 ........p.....y.
62800020: 02e0 005a 0421 0060 0000 0000 0000 0000 ..Z.!.`.........
62800030: 0000 0000 0020 0000 0800 0000 1b88 4073 .... .........s@
62800040: 0000 0000 0000 0000 5709 0002 ffff ffff .........W......
62800050: ee09 0002 1060 0000 ea09 5c08 5000 8028 ....`......\.P(.
62800060: ea09 6005 8080 0000 6108 4000 da79 e7f9 ...`.....a.@y...
62800070: ffff ffff ffff ffff ffff ffff ffff ffff ................
Generated RCW (does not boots)
=> md.w 60000000
60000000: 55aa 55aa ee01 0001 0806 0a00 0000 0000 .U.U............
60000010: 0000 0000 0000 0000 0070 0000 0000 0079 ........p.....y.
60000020: 02e0 0050 0401 0060 0000 0000 0000 0000 ..P...`.........
60000030: 0000 0000 0020 0000 0800 0000 1b88 4073 .... .........s@
60000040: 0000 0000 0000 0000 5709 0002 ffff ffff .........W......
60000050: ee09 0002 1060 0000 ea09 5c08 5000 8028 ....`......\.P(.
60000060: ea09 6005 8080 0000 6108 4000 3569 b238 ...`.....a.@i58.
60000070: 0000 0000 0000 0000 0000 0000 0000 0000 ................
Uboot being used:
U-Boot 2015.01+ls1+g3281947 (Jul 30 2015 - 20:01:52)
CPU: Freescale LayerScape LS1021E, Version: 2.0, (0x87081120)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 70000000 00007900 e0025a00 21046000
00000020: 00000000 00000000 00000000 20000000
00000030: 00080000 881b7340 00000000 00000000
Board: LS1021ATWR
CPLD: V2.0
PCBA: V1.0
VBank: 0
I2C: ready
DRAM: 1 GiB
Using SERDES1 Protocol: 112 (0x70)
Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0
QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1
Flash: 128 MiB
MMC: FSL_SDHC: 0
EEPROM: NXID v1
PCIe1: Root Complex no link, regs @ 0x3400000
PCIe2: Root Complex no link, regs @ 0x3500000
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
SATA link 0 timeout.
AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc
scanning bus for devices...
Found 0 device(s).
SCSI: Net: eTSEC2 is in sgmii mode.
eTSEC1, eTSEC2, eTSEC3 [PRIME]
解決済! 解決策の投稿を見る。
Hi Luc!
Thank you for reporting this issue. The fix was implemented and should be visible starting with QCVS 4.5.
Best regards,
Mihai Surdeanu
When will it be available on your web site?
Right now, it still proposes to download 4.4.1.
Hi Luc!
We are planning to release QCVS 4.5 in ~10 days from now.
Thank you.
Unfortunately, PBL generated with QCVS will set the reserved bits to a default value (which may be wrong in some cases). We have in mind to add a new feature, to preserve the values of reserved bits to the one to imported PBL.
Also, I have one question: Have you get this PBL from SDK or from other source?
Adrian
It is what I found on the board when I received it from NXP/freescale (or from the reseller we use).
When can we expect to have a fix that you describe?
Is there an RCW that would work with QCVS and the LS1021ATWR?
A fix will be provided in a future QCVS release. All RCWs from SDK should work fine with QCVS.
Adrian