Connet MPC8245 to CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connet MPC8245 to CodeWarrior

1,313件の閲覧回数
xuchaoli
Contributor I

I have config the MPC8245 with 32-bit width SDRAM, Atell me that USB TAP only support 64-bit width SDRAM,so can you tell me what TAP can use to connect  32-bit MPC8245?

 

My MPC8245 can't connect to USB TAP 114189_114189.bmp未命名.bmp

ラベル(1)
0 件の賞賛
10 返答(返信)

869件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello xuchao li,

I never heard of that.

Regards

Lunmin

0 件の賞賛

869件の閲覧回数
xuchaoli
Contributor I

I need to connect my board,but you said that that kind of solution is not accessable, so would youtellme if there any solution I can get. Thank a lot.

0 件の賞賛

869件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello xuchao li,

Did you try CCS commands or only CW?

Regards

Lunmin

0 件の賞賛

869件の閲覧回数
xuchaoli
Contributor I

I don't know what is CW or CCS commands . would you give me more detailed description ?

0 件の賞賛

869件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello xuchao li,

May I know your CCS version?

In the CCS console window enter command

show version

You should see the version number in the CCS console window.

BR

Lunmin

0 件の賞賛

869件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello xuchao li,

CW is CodeWarrior, CCS is CodeWarrior Connection Server, invoking from Start->All Programs->Freescale CodeWarrior->CW for XXX->CodeWarrior Connection Server.

So you have no problem to connect target?

BR

Lunmin

0 件の賞賛

869件の閲覧回数
xuchaoli
Contributor I

Thanks a lot .the connect qusention is asoved,the reason is Iconenect the JTAG signal wrong,I made a mistake

0 件の賞賛

869件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Good to know, and thanks for sharing reason.

0 件の賞賛

869件の閲覧回数
xuchaoli
Contributor I

I use the edition of CodeWarrior  is  8.8,and my emulator is USB TAP.

Access the memoy of any space,like PCI、SDRAM、Flash,the data is same ,and if the address is end by 0x4,or by 0xc,like 0x0000_01024、0xFF00_000C,the data is all "00000000".if the address is end by 0x0,or ox8,the result is correct.So I conjecture that mybe USB TAP don't support the MPC8245 in 32-bit mode ?

0 件の賞賛

869件の閲覧回数
Pavel
NXP Employee
NXP Employee

The MPC8245 processor core has a selectable 32- or 64-bit data bus and a 32-bit address bus. See the Section 1.2.4 of the MPC8245 User’s Manual.

CodeWarrior 8.8 supports only 32-bit data bus.

CodeWarrior 8.6 supports 32-bit and 64-bit data bus. CodeWarrior 8.6 does not support USB TAP.

It is mistake in CodeWarrior 8.8.

Have a great day,

Pavel

0 件の賞賛