CodeWarrior Coldfire SE license won't allow debug from SRAM on 5211

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Coldfire SE license won't allow debug from SRAM on 5211

1,654件の閲覧回数
Neilp
Contributor I
Hi All.

I'm having a wierd problem with Codewarrior for CF SE. I created an application for the M5211DEMO board using MicroAPL's CFInit application.  can get the application to run fine using the 'boot from ROM/flash' target, but if I try loading the application into ram using 'console debug (SRAM)' or 'UART debug (SRAM)' I get the following license error: "The debugger download size has been exceeded. This is specified in the license file." Looking at the actual Console Debug(SRAM).elf.s19 file it is only 11k in size?? Is there a limitation on ram target size in the SE version??

Regards,
Neil.
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

522件の閲覧回数
CrasyCat
Specialist III
Hello
 
I am not sure you will get an answer to this one in the forum.
 
I would suggest you to submit a service request for that.
Click here to submit a service request.
 
Make sure to attach a project reproducing the trouble to the service request.
 
CrasyCat
 
0 件の賞賛
返信

522件の閲覧回数
Neilp
Contributor I
Ok, Will do. Thanks CrasyCat

Neil.

0 件の賞賛
返信