CodeWarrior 7.1 vs 7.1.1 vs 7.1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 7.1 vs 7.1.1 vs 7.1.2

1,363 Views
theJoel
Contributor III

Hello,

 

Which is 'newer' CW 7.1 Build 14, or CW 7.1.1a Build 9?

 

I get slightly different final output, but no immediately visible difference in execution of my application.

 

 

CW 7.1.2 has MAJOR problems with mcf5270 and is not an option.

 

 

Cheers,

Joel.

Labels (1)
0 Kudos
Reply
2 Replies

379 Views
Adam
Contributor III

Hi, 7.1.1a is newer than 7.1.

 

Yes, 7.1.2 has major issues which every target with standard C things.

0 Kudos
Reply

379 Views
theJoel
Contributor III
Thanks. That makes sense... I just wasn't sure with the "Build 9" vs "Build 14" Cheers, +Joel.
0 Kudos
Reply