CodeWarrior 7.1 vs 7.1.1 vs 7.1.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 7.1 vs 7.1.1 vs 7.1.2

1,229件の閲覧回数
theJoel
Contributor III

Hello,

 

Which is 'newer' CW 7.1 Build 14, or CW 7.1.1a Build 9?

 

I get slightly different final output, but no immediately visible difference in execution of my application.

 

 

CW 7.1.2 has MAJOR problems with mcf5270 and is not an option.

 

 

Cheers,

Joel.

ラベル(1)
タグ(1)
0 件の賞賛
2 返答(返信)

245件の閲覧回数
Adam
Contributor III

Hi, 7.1.1a is newer than 7.1.

 

Yes, 7.1.2 has major issues which every target with standard C things.

0 件の賞賛

245件の閲覧回数
theJoel
Contributor III
Thanks. That makes sense... I just wasn't sure with the "Build 9" vs "Build 14" Cheers, +Joel.
0 件の賞賛