CW & u-boot debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW & u-boot debug

6,744 次查看
Igor
Contributor III
Hi all,
I have installed CW Dev Studio (Power architecture, Professional edition & Linux Application edition, v8.8, Build 70921) on a WinXp based computer. Secondly, on a Fedora core based host computer, I have cross compiled u-boot 1.1.6 for mpc8313rdb board (toolchain gcc-4.0.2+e30c3/glibc-2.3.6).
 
The issue is that I want to debug u-boot using CW (and USB TAP) but breakpoints "do not work".
 
This is what I've done:
Within CW, I have done a "File | Open" on the u-boot elf image.
CW has created a project for that elf file (it has not found libgcc2.c file so it gives me a "warning" message).
Once the project is created I have set the target CPU type in the EPPC Debugger Settings panel and a register init file (8313RDB_uboot_init_Linux.cfg).
Any Advice? Do I have to compile u-boot in a particular manner?
Thanks a lot in advance,
Igor
标签 (1)
标记 (1)
0 项奖励
回复
9 回复数

1,791 次查看
huangxianguo
Contributor I
I think the libgcc2.c is not neccessary if you have compiled the u-boot. you can skip it. you can find it at the libc source.
0 项奖励
回复

1,791 次查看
AshishAgarwal
Contributor III

I receive an answer regarding my Servie request to Freescale is like below.

 

 

uboot debugging
------------------
This is not supported for 8536 yet.  It will not be supported until the June 22 release (CW EPPC 8.8.3). 

 

Got stuck with in development cycle. :smileysad:

 

but now one thing we can do is insert printf statements in the u-boot source to debug it..

 

i know it is hard to compile source every time and write it to the Flash but it is the only way i am doing :smileyhappy:

 

if you know any other bright way to do the same .. 

 

v- -v suggest me :smileyhappy:

0 项奖励
回复

1,791 次查看
AshishAgarwal
Contributor III

Freescale support comments :

 

uboot debugging

----------------

 

This is not supported for 8536 yet.  It will not be supported until the 2009, June 22 release (CW EPPC 8.8.3).

0 项奖励
回复

1,791 次查看
huangxianguo
Contributor I

Fortunately, i have known how to debug.

 If you

1.want to stop at FLASH breakpoint:

a.  check the option "use Target Initilization File", and locate the file"Program Files/Freescale/CodeWarrior PA V8.8/PowerPC_EABI_Support/Initialization_Files/PQ2/83xxRDB_init_debug_uboot.cfg"

b.  non-check the option "Alternate Load Address"

 

2.want to stop at RAM breakpoint:

a. non-check the option "use Target Initilization File"

b. check  "Alternate Load Address" in terms of the section: " Debugging the U-Boot Bootstrap Firmware" in the document"/Program Files/Freescale/CodeWarrior PA V8.8/Help/Pro_&_Linux_App_Edition_Targeting_Manual.chm

c. set Hardware Breakpoint

 

other settings follow the .chm file in step.

0 项奖励
回复

1,791 次查看
AshishAgarwal
Contributor III

Hello huangxianguo

 

Thanks for your kind reply. it true what you commented, is steps for the debuging of U-boot.

 

But here i mentioned that i want to debug the MPC8536DS version u-Boot 1.3.4.

 

and indeed i did the debugging of MPC8544 successsfully before the procedure written abov. but in my case right now i am not able to get rid from "libgcc2.c"file missin.

 

it is the case when we open ****.elf file. i made sure about the process written there in mannual.

 

what i am looking is if there is any FLAG setting in the Makefile i am missing that generates "libgcc2.c" file warning. that stops me to halt at breakpoints.

 

0 项奖励
回复

1,791 次查看
huangxianguo
Contributor I
I encounted the same issue-- lack of libgcc2 and breakpoint unreachable, and don't know how to resolve. i have operated with the instructor step by step, but that's useless still. lgor, whether you  have resolved this issue? can you give me some tutorial?
0 项奖励
回复

1,791 次查看
Igor
Contributor III

Some time has passed...Sorry but the only thing I remember is that I religiously followed the document's procedure.

 

Igor

0 项奖励
回复

1,791 次查看
AshishAgarwal
Contributor III

I am using MPC8536DS Evaluation environment.

nowhow i was able to get working configuration [JTAG] file for the 8536.

 

i too facing same problem. :smileymad:

when i compile the u-Boot over ltib tool as described in "Pro & Linux App Edition Targeting Manual.pdf" => Debugging the U-Boot Bootstrap Firmware

 

step by step following of guide still not working for me :smileysad:

 

1 point i am not sure about is 【manual Note】

 

"NOTE If you are using an LTIB BSP, you may need to change the optimization flag of
the U-Boot CFLAGS argument in this file: install/ltib/config/platform/boardName/.config file."

 

what i have to set there and with which flag?

 

i.e there is Flag named as 

CONFIG_TOOLCHAIN_CFLAGS=""

becuase this is a auto genereted file from ltib config tool, so i changed this from that tool as "-O2"

is it wrong anywhere or i loosing something @?@;

 

here what i have to do otherwise?

please help me out if anybody resolved this issue anyhow. :

 

u-Boot code compiled successfully but when i tried to open elf file in the C, it is giving me warning about "libgcc2.c" file not found.

 

The command i am using for compiling is  :robotmad:

./ltib -m scbuild -p u-boot-1.3.4-mpc8536ds.spec

 

is it Okie ?

 

libgcc2.c file does not exists or it may not be genereted.

 ---

 

:smileytongue:

 

Ashish Agarwal

"There's no ceiling on effort!"

0 项奖励
回复

1,791 次查看
J2MEJediMaster
Specialist I
Consult the Pro & Linux App Edtion Targeting Manual  in CodeWarrior's Hlpe directory. In ths manual's Working with the Debugger chapter, locate the section, Debugging the U-boot Bootstrap Firmware, and follow its directions. It describes in detail what you must do to build the U-boot code and download it. HTH,

---Tom

0 项奖励
回复